Configuration files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuration files

Jump to solution
682 Views
leccy
Contributor III

Codewarrior 10.1 for Kinetis

 

I need to have a number of different configurations for each project.

 

Each configuration will have a number of configuration-specfic #include files.  Some of these files will be generated by pre-build scripts from e.g. .BMP files.  If I put these .BMP files in the configuration folder, and start a Clean/Build, the files are destroyed and the script fails.

 

I found this process easy to do with IAR, but I am struggling to find settings, processes etc that allow this to work.

 

Can someone please point out the obvious!

 

Thanks

Alex

Labels (1)
0 Kudos
Reply
1 Solution
524 Views
CrasyCat
Specialist III

Hello

 

  When you perform a Project Clean, Eclipse will delete the whole build directory.  

  So only files that are re-created by a Project Build should be stored in there.

 

  If you need to keep the .bmp file after a Clean Project you need to store them in a folder outside of the build directory.

  You can for example create a directory bmp_files and add one sub-directory for each build configuration you are using.

  Then store the .bmp files in the appropriate sub directory.

 

  If the directory bmp_files is located in the project directory tree, make sure to exclude the folders holding .bmp for other

  configurations from a particular  build config.

 

  This is quite easy. To remove a folder from a build configuration:

       - Inside of the CodeWarrior Project view, click right on the folder name

       - In the drop down menu select Properties.

       - Activate the C/C++ Build page 

       - Check Exclude resource from build.

 

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
525 Views
CrasyCat
Specialist III

Hello

 

  When you perform a Project Clean, Eclipse will delete the whole build directory.  

  So only files that are re-created by a Project Build should be stored in there.

 

  If you need to keep the .bmp file after a Clean Project you need to store them in a folder outside of the build directory.

  You can for example create a directory bmp_files and add one sub-directory for each build configuration you are using.

  Then store the .bmp files in the appropriate sub directory.

 

  If the directory bmp_files is located in the project directory tree, make sure to exclude the folders holding .bmp for other

  configurations from a particular  build config.

 

  This is quite easy. To remove a folder from a build configuration:

       - Inside of the CodeWarrior Project view, click right on the folder name

       - In the drop down menu select Properties.

       - Activate the C/C++ Build page 

       - Check Exclude resource from build.

 

CrasyCat

0 Kudos
Reply
524 Views
leccy
Contributor III

CrasyCat

 

Many thanks for your reply.

 

That is working fine now.

 

Alex

0 Kudos
Reply