Create an update partition and switch to boot from there

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create an update partition and switch to boot from there

808 Views
dvega
Contributor II

I have a iMX8mp board. I created a yocto image and works just fine. It creates 2 partitions bootfs and rootfs. I want to create a 3rd partition rootfs2. Clone rootfs partition to rootfs2 into the device in the extra space. And boot from there. This is to do over the air updates. When an update fails to boot then just switch and boot from the original one.

On as raspberry pi is actually very simple. You just open the cmdline.txt file on the boot partition. Modify the root=PARTUUID=XXXXXX-XX to the values you want.

The iMX8mp board uses uboot. Seems that it is possible to modify it to achieve this. However I was not able to find much documentation on how to do this.

1 Reply

605 Views
bgaurav1718
Contributor III
I am facing similar problems. Please share the solution if you found one.
0 Kudos
Reply