i.MX Solutions Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Solutions Knowledge Base

Labels
  • General 294

Discussions

Sort by:
This video shows how the Crank Storyboard application framework is well suited to run on our i.MX7 Nitrogen7 board. Demo details This demonstration is based on the following: Nitrogen7 board​​ 800×480 LCD display​ Resistive touch Yocto Jethro release Linux kernel 3.14.52 Crank Software details Crank Software Inc. is an innovator in embedded graphical user interface (GUI) solutions. Their products and services enable R&D teams and UI Designers to quickly and collaboratively develop rich animated user interfaces for resource-constrained embedded. The demo above relies on the Crank Storyboard Engine which is: Multi-platform Supported on Linux, Android, QNX, WindowsCE among others Built for embedded Storyboard Embedded Engine scales from low-end to high-end processors 3D optimized For higher end products embedding a GPU For more information, please visit: https://boundarydevices.com/crank-software-demo-on-nitrogen7/
View full article
Imx6 can output lvds direct.But the lvds-wire is too  expensive to buy. So they can cannect ds90ub947 serializer to applied in automotive instrumentation. By the way, it need a ds90ub948 deserializer in the remote which cannect a lvds displayer. The attachment is the driver of ds90ub947/948 for linux.It can  support linux 3.10 and above.It was verified working on linux 3.10.53 and imx6q. The attachment list: ds90ub947.c ds90ub947.h readme.txt You can follow the readme to use it. This driver was barely in embryo.You should modify it according to your application. Sometime, it very looks like the ds90ub913/914 and max9286/96705.
View full article
Adeneo Embedded, a Freescale Connected Proven Partner, continues its commitment in working with Freescale on its i.MX product line. With Freescale’s announcement of the i.MX product roadmap (Freescale i.MX Roadmap blog) and Adeneo Embedded’s latest releases of Operating System BSPs for the i.MX6 platforms, the two companies strengthen further their collaboration and capabilities by bringing best products and services to their customers.   Adeneo Embedded has developed Android, Linux, QNX and Windows Embedded Compact BSPs for a wide range of Freescale’s i.MX products. Adeneo Embedded is the first company to develop the Windows Embedded Compact 2013 BSP on the i.MX6 platforms, supporting SABRE SD Board and SD Platform from Freescale, as well as many different 3 rd party boards including SABRE Lite based platforms and various System On Modules. Adeneo Embedded is also the official i.MX6 training partner of Freescale, jointly conducting about 60+ trainings each year across America and Europe .   Adeneo Embedded is pleased to see Freescale announcing the upcoming i.MX7 and i.MX8 series and will help customers designing products based on these new technologies with a complete portfolio of solutions and services to support the integration of Embedded OS, Middleware and Connected Applications.     About Adeneo Embedded Adeneo Embedded provides system integration, design, support and training services to companies seeking world-class expertise in embedded solutions using high-performance architectures. For over 10 years, Adeneo Embedded has helped clients, in all stages of development; create profitable, feature-rich products that incorporate software and hardware solutions based on Windows Embedded, Windows Phone and Windows 8 operating systems. Close working partnerships with industry-leading silicon and software vendors allow Adeneo Embedded to apply its experience to a wide range of embedded solutions for the automotive, industrial, medical,  multi-media, navigation,  networking, mobile and wireless markets. Adeneo Embedded has a global sales and support network backed by engineering offices in North America and Europe.   © 2013 Adeneo Embedded. All Rights Reserved. All other brands or product names are the property of their respective holders   Further information For more information about Adeneo Embedded competences, products and services around Windows Embedded technologies:   visit Adeneo Embedded dedicated web site                 www.adeneo-embedded.com Adeneo Embedded General sales contact                    sales@adeneo-embedded.com   For a local contact in   Central Europe, contact Michael Heinz                      mheinz@adeneo-embedded.com South&North Europe, contact Jeremy Delicato         jdelicato@adeneo-embedded.com America, please contact Mike Ruiz                            mruiz@adeneo-embedded.com Asia, please contact Vijay Raisinghani                       vraisinghani@adeneo-embedded.com
View full article
The Solution of the Month is the Freescale i.MX6 based Qseven QMX6 a collaboration by Adeneo Embedded and congatec AG Adeneo Embedded is proud to announce its collaboration with congatec on the Freescale i.MX6 based Qseven QMX6 computer-on-module. Congatec is a leading supplier of industrial computer-on-modules supporting the ETX, XTX, COM Express and Qseven form factors.  The conga-QMX6 module was designed to the industry standard Qseven form factor. congatec’s products can be used in a variety of industries and applications, such as industrial automation, medical technology, automotive supplies, aerospace and transportation. Following the design-in phase, customers are given support via extensive product lifecycle management.   Adeneo Embedded has jointly developed and maintains Windows Embedded Compact, Linux and Android BSPs for the conga-QMX6 Qseven module. The combined expertise of both companies on h/w and s/w provides unmatched support to customers in enabling them to move quickly with their designs.   Adeneo Embedded continuously updates the BSP with feature updates and improvements. More information about this product and also other Freescale products supported by Adeneo Embedded can be found at http://www.adeneo-embedded.com/Products/Board-Support-Packages/Congatec-conga-QMX6-BSPs Contact Adeneo Embedded @ sales@adeneo-embedded.com
View full article
Adeneo's entry for solution of the month in collaboration with Congatec
View full article
Watch the demo of Color Segmentation using e-CAM130_iMX8 - 13MP Autofocus Camera Board for i.MX8. e-CAM130_iMX8 is a 13MP 4-lane MIPI CSI-2 autofocus color camera board for i.MX8 family of processors. The e-CAM130_iMX8 camera board is interfaced directly to the CSI-2 MIPI interface on the Variscite's DART-MX8M Evaluation kit (VAR-DVK-DT8M). The iHDR (interlaced High Dynamic Range) support helps to capture good quality images in both high and low illumination. e-CAM130_iMX8 also comes with a high-performance Image Signal Processor (ISP) that performs all the Auto functions (autofocus, auto white balance, auto exposure control).
View full article
http://www.youtube.com/watch?feature=player_embedded&v=-qezzzutBeo   Uploaded by dai0ane on Aug 4, 2010 Http streaming of a mp3 file on Android running on iMX51 EVK Category: Science & Technology License: Standard YouTube License  
View full article
i.CORE RQS M6S/DL/DQ i.Core RQS M6S/DL/D/Q is the latest powerful i.MX6 solution provided by Engicam in micro Q7 format. Equipped with single,dual light,dual or quad Cortex-A9 core and different size of memories The full scalability of modules allows to create multiple products with different performance in a very short time to Market. Features Memories 1GB 64bit DDR3-1066  for i.Core RQS M6Q 512MB 64bit DDR3-1066  for i.Core RQS M6D 512MB 64bit DDR3-800  for i.Core RQS M6DL 256MB 32bit DDR3-800 for i.Core RQS M6S 4 GB e-MMC Graphics and Multimedia 2x LVDS output 1x HDMI output Up to three simultaneous display driving support ( i.Core M6Q/D only) Up to two simultaneous display driving support ( i.Core M6S/DL only) Dual display up to WUXGA (1920x1200) and HD1080 OpenGL/ES 2.x 3D accelerator with OpenCL/EP support and OpenVG1.1 acceleration Multi-format HD1080 video decode and encode Peripherals SD Card interfaces USB OTG HS, USB HS HOST, Uart, I2C, I2S, PCI Express SATA 3Gbps (i.Core M6Q/D only) Ethernet 10/100/1000 On board WiFi option available Dimensions Standard uQ7 http://www.engicam.com/en/products/embedded/som/standard/i-core-rqs-m6s-dl-d-q                
View full article
澳洲大学挂科怎么办联系QQ1252839746,考试挂科作弊、GPA低被开除退学、收到学术警告。澳洲大学2018 S1的Final成绩已经在陆续发放了,拿到成绩的时候,有些人难免会沮丧,复习了的内容没考,考的内容没复习,所以就有科目理所应当的挂科了…… 澳洲大学向来是宽!进!严!出!随着成绩的公布,小伙伴们都在问挂科了到底该怎么办?一起来了解一下不同情况的挂科该如何处理吧! 同一学期挂科科目挂科小于等于50% 什么叫挂科科目小于等于50%呢?各大学的课程设置都是一学期4门课,如果你在一学期中挂了1-2门,但是还没有出现double fail(一科已经连续fail两次以上),那么学校不会对你有任何行动,下学期一定要争取4门全部Pass来弥补! 同一学期挂科科目挂科大于等于50% 大于等于50%的意思就是如果在一学期中挂了2门以上课程,那一般学校就会采取第一次行动了,会对你发出一封警告信! 学校出勤率低于80% 和挂科无关,但非常重要。如果同学们在一学期中,因各种原因出勤率不满80%的,并且针对这过低的出勤率没有合理的理由,学校也会先对你做出警告需要解释,如果理由没有被学校接受,学校也有资格将你上报移民局,移民局可以会跟据情况取消签证。 努力学习却还是挂科 如果是平时十分努力却还是掌控不了挂科的同学门要及早正视自己的问题,对自己挂科的原因进行总结,可能是由于专业不适合,学习能力不够,学校和你的学习理念存在差异……而这类学生最重要的就是正视自己的情况考虑转学校或者是换专业。 警告信解释 当你不幸收到开除警告信后,书面解释的质量非常重要。 首先,解释列举的原因,一定是不可控的因素,由此导致的学习成绩差;接着表明自己坚信可以完成学业,并列举理由;最后认真的规划应该如何去克服困难,努力提高成绩。 如果以身体健康原因作为理由,必须准备辅助材料,如医生开具的证明等,一同上交。校方受理后会决定十分需要召开听证会,听证会后即会给出解释结果。 转校 这里需要提醒小伙伴们如果被公立大学开除,则无法转到其它公立大学继续学习,只能转到各种私立大学或学院,但可以在收到学校警告信后,马上开始准备转学事宜,在开除程序正式开始之前申请转学。 转学 若未读满6个月的课程就申请转学,首先需要获得想转学学校OFFER,然后向在读学校申请Release letter(放行信),在读学校会根据转学政策和程序审核申请,再决定是否发放Release letter; 如果已经在主课学校就读超过六个月,一般学校都会同意学生的转学申请。 在澳洲挂科除了昂贵的学费外,还有可能会面临强制退学和取消学生签证,并且3年都不得进入澳洲,所以要谨慎对待每次考试,澳洲大学挂科改成绩(Q1252839746)挂科GPA成绩修改,解决被退学开除等问题。
View full article
iWave offers i.MX6 Qseven modules with latest 3.10.17 based Linux kernel with Yocto support. This official Yocto release is based on 3.10.17 kernel. The BSP will support for all the variants of i.MX6 CPU, i.e Quad, Dual, Dual Lite and Solo Qseven modules. The alpha release for the same is now available on request. This release supports the below features on our Qseven Development Platform: Freescale i.MX6 Q/D/DL/S CPU DDR3 SDRAM SPI Boot flash eMMC Flash Debug Console SD Ports USB Ports Ethernet PCIe HDMI 7”LVDS display For further information or enquiries please write to mktg@iwavesystems.com or visit our website www.iwavesystems.com
View full article
Hi All, One of my recent work with IMXRT Series MCU's, A Simple Drum Pad Proto designed with IMXRT Crossover platform MCU's and Capsense touch. For more details about the project and source. checkout here https://www.hackster.io/ashokr/imx-rt-drum-pad-a8c1cd Thanks Ashok R Embedded Club (@embeddedclub) • Instagram photos and videos #nxp 
View full article
iWave provides Android Lollipop and Linux 3.14 kernel BSP upgrades for its i.MX6 based products. iMX6 Board: From the launch of i.MX6 application processors, iWave Systems, a global leading SOM supplier has launched many variations of i.MX6 CPU modules and an SBC board catering to Industrial, automotive and medical applications. Complying with the Qseven R2.0 specification, the i.MX6 Q7 SOM supports industrial grade operation with 70mmx70mm size. The i.MX6 MXM SOM supports automotive grade i.MX6 CPU and the automotive specific interfaces with 314 pin MXM2 connector pinout in 85mmx85mm form factor. The recently launched i.MX6 SODIMM SOM module supports both commercial & industrial operating temperature with very compact form factor of 67.6mmx37mm. iMX6 Board Single Board Computer: Measuring 100mmx70mm, the Pico ITX size i.MX6 SBC board supports on-board connectors for all the i.MX6 interfaces with option to expand IOs through expansion connector.  All these three different form factor System on Modules and Single Board Computers are supported with different i.MX6 CPU variations such as Quad, Dual, Dual Lite & Solo. Besides this i.MX6 Qseven modules also supports i.MX6 Quad Plus and i.MX6 Dual plus CPU configurations. To enable quick prototyping of these different form factor SOMs, iWave systems supports independent development kit variation for each form factor SOMs with Linux, Android and WEC7* BSP support. These development kits help customer to save up to 60% of new product development cycle sothat the quick time to market can be achieved. All these i.MX6 products are getting Android Lollipop and Linux 3.14 kernel BSP upgrades which will be available for customers by the first quarter of 2016.
View full article
http://www.youtube.com/watch?v=qWUd4TAEqTM&feature=player_embedded   Uploaded by Charbax on Jun 20, 2011 Konstantinos Margaritis is a Senior Software Engineer at San Antonio based Genesi, he talks about how Genesi is pushing Linaro forward to recompile all the apps and everything around Linux to use hard float, to re-optimize floating point applications on ARM Powered Desktop/Laptop designs. Watch this video interview to find out how Genesi is doing these software optimizations on Debian for the i.MX51 and i.MX53 platforms in their ARM Powered Smartbook designs. How soon are ARM Powered laptops going to have enough performance optimizations in them to demonstrate that ARM is fast enough to power Desktop/Laptop designs so that every consumer can be satisfied with the performance? Category: Science & Technology License: Standard YouTube License  
View full article
iWave Systems, one of the early adopters of i.MX6 technology has designed i.MX6 based network switch/router solution. The task involved the design and development of a custom carrier card for our i.MX6 Qseven Module, the carrier card also consists of microcontroller. Together with the i.MX6 Qseven module and carrier card, the solution provides router capabilities. i.MX6 based Router Solution The carrier card was designed by iWave to meet the network Router requirement using iWave’s i.MX6 Qseven SOM. The Wi-Fi modules and GPRS modules (mini PCIe form factor) were interfaced to the PCIe 2.0. With the Gigabit Switch connector, the board supports four RJ45 connectors. Totally, there are six Mini PCIe slots available, accommodating both PCIe and USB signals. Microcontroller, in the carrier card, monitors parameters like voltage levels and power status. It also provides user interface by controlling appropriate LED’s to indicate which mini PCIe module is active. Block Diagram iWave’s i.MX 6 Qseven SOM is connected to the PIC Microcontroller through I2C. Connection is in such a way that iMX6 processor, as a Master and PIC microcontroller, as a Slave. Master and Slave to communicate effectively, iWave has designed a unique customized Communication Protocol in which master (iMX 6) will control the peripherals connected to slave (PIC) through protocol commands. iWave also implemented a software in our Qseven  module that enables the upgrade of the microcontroller firmware. For further information or inquiries please write to mktg@iwavesystems.com or contact our Regional Partners website: www.iwavesystems.com
View full article
Digital Signage is an application that the i.MX6 processor is the perfect fit. With the hardware encoding and decoding, video outputs and inputs and processing power, using the i.MX6 for Digital Signage is very popular!
View full article
These videos demonstrate an example application of a fully cloud-enabled and location-aware mass transport demo built on Freescale's i.MX5x platform with a HD passenger information display, PCAP touch enabled driver control display, and mobilde device (Android phone) integration. The demo showcases how Android provides the potential of significantly shortening the development cycle and accelerating your time-to-market. The demo is based on the Digi ConnectCore i.MX53 System-on-Module solution and was built using our Embedded Application Development Kit for Android (Gingerbread). Smart Tech for Passenger Buses by Digi International - Design West (ESC) 2012 - YouTube - The ARM video interview at Design West Android Bus Demo - YouTube  - The official Digi video overview Visit www.digiembedded.com for additional information, including a special i.MX53 Android Development Kit kit offer for $199. --- VDC Research Awards Digi Best of Show at Embedded World 2012 for Android Application Development Kit with iDigi Device
View full article
MYIR has released a cost-effective and power-efficient ARM Evaluation Kit (EVK) MYD-IMX28X for Freescale i.MX28 family of multimedia applications processors which has an ARM926EJ-S Core, with speed up to 454 MHz. The board can support running Linux operating systems, which allows developers to use it as an i.MX28 reference platform to quickly start their own design. The board takes full features of the i.MX28 ARM processor and has exposed a comprehensive set of peripherals and connectivity options to make the board suitable for smart gateways, human-machine interfaces (HMIs), handheld devices, scanners, portable medical, experimental education and more other industrial applications. The MYD-IMX28X Development Board is using the MYC-IMX28X CPU module as the heart of the system which is an ARM9-based system-on-module (SOM) integrated with the i.MX28 processor, 128MB DDR2 SDRAM, 256MB Nand Flash and Ethernet PHY. It is connected to the base board through two 1.27mm pitch 80-pin connectors. The base board has extended many peripherals and interfaces through headers and connectors, featuring 1 x RS232, 1, Debug, 2 x USB ports, up to 2 x Ethernet, 1 x CAN, 1 x RS485, TF, Audio, LCD, JTAG, etc. MYD-IMX28X Development Board MYC-IMX28X CPU Module MYIR offers the board with Freescale i.MX283 or i.MX287 ARM9 CPU by default; user can integrate a different MYC-IMX28X CPU module on the same base board, thus making two variants of i.MX28 evaluation boards. MYD-IMX283 Development Board – with MYC-IMX283 CPU Module for Freescale i.MX283 MYD-IMX287 Development Board – with MYC-IMX287 CPU Module for Freescale i.MX287 The MYD-IMX283 and MYD-IMX287 boards only have a few differences as described in below table: Model MYD-IMX283 MYD-IMX287 Processor i.MX283 i.MX287 CAN 0 2 Ethernet 1 2 The MYD-IMX28X board comes with Linux2.6.35 software packages, detailed documents, necessary cable accessories as well as optional 4.3- and 7-inch LCD (with touch screen) to provide a complete Freescale i.MX28 starter kit and enable a quickly start of evaluation of i.MX28 family applications processors.
View full article
Single Board Computers have always enjoyed serious attention in the field of Embedded Systems design. Ever since its introduction, its main intention was to devise a computer to inspire students to take up many new projects to explore the rich and wide world of Embedded Systems. With products like i.MX6 Pico ITX SBC, i.MX50 Quick Start Board, i.MX27 & PXA 270 SBCs, we at iWave Systems, are clearly a global competitor when it comes to promoting powerful ARM Cortex Single Board Computers. i.MX6 Pico ITX SBC: iWave's i.MX6 Dual Lite/Solo based Pico ITX SBC comes with all standard interfaces loaded into a single board with ultra-compact yet highly integrated platform that can be utilized across multiple embedded PC and industrial designs. It also provides an expansion header through which interfaces can be used according to their applications, measuring at just 100mm x 72mm. Pico ITX Advanced Learning Platform: As our product was aimed at inspiring young engineers to take up several projects in the field of Embedded Systems design iWave systems came up with a versatile and well equipped peripheral daughter board which can be plugged to the iWave’s i.MX6 Pico ITX SBC. This peripheral daughter board provides the extension to the I.MX6 Pico ITX board to evaluate several new display, sensor, communication & IO interfaces. The i.MX6 ARM Cortex A9 Pico ITX SBC with peripheral daughter board forms a powerful starter kit for the university students to plug & play several hardware & software components and make many new innovative concepts. The main interfaces supported by peripheral daughter board are as follows: Display Interfaces: A combination of a 7” TFT LCD display, 16x2 Character LCD and a 4 digit 7 segment display for display centric applications. Communication Interfaces: Additional RS232 & CAN ports for standard communication between external devices. Sensor module: Aimed specifically for engineering project works with various sensors like Ambient light sensors, Proximity sensors, Temperature sensor, Accelerometer and Magnetometer Motor Interface: A single driver that is capable of either driving two DC motors or a single Stepper motor Keypad Interface: Keypad scanner and a 4x4 keypad connector support External interfaces: The peripheral daughter board also following several interfaces CMOS camera interface support available on 17x2 row connector MIPI DSI interface support available on 10 pin MIPI connector SPI interface available on 6 pin SPI header Dual UART interface available on the 6 Pin UART header i.MX6 based Pico ITX Educational Kit For more information please contact: mktg@iwavesystems.com Website: www.iwavesystems.com
View full article