i.MX RT1170 DVFS Demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX RT1170 DVFS Demo

i.MX RT1170 DVFS Demo

Dynamic voltage and frequency scaling (DVFS) is a power management technique that allows dynamically reducing power consumption of a CPU by dynamically scaling down supply voltage and CPU frequency. Because the internal DCDC of the i.MX RT1170 cannot cover the needed maximum current requirement at the junction temperature of 125 °C, the DVFS technique can be used to reduce current drain for compatibility with the internal DCDC. Lowering the processor frequency dynamically can help reduce the chip input current demand and ensure that the chip can continue to work at the junction temperature of 125 °C.

The demo is attached. Only IAR and armgcc versions are enabled.

The corresponding Application Note can be downloaded in the below link.

https://www.nxp.com/docs/en/application-note/AN13267.pdf

附件
无评分
版本历史
最后更新:
‎05-31-2021 01:56 AM
更新人: