Unboxing MYD-JX8MX NXP i.MX 8M based Development Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unboxing MYD-JX8MX NXP i.MX 8M based Development Board

Unboxing MYD-JX8MX NXP i.MX 8M based Development Board

The MYD-JX8MX development board is a versatile platform based on the NXP i.MX 8M Quad processors which feature 1.3GHz quad ARM Cortex-A53 cores and a real-time ARM Cortex-M4 co-processor and provide industry-leading audio, voice, and video processing for applications that scale from consumer home audio to industrial building automation and mobile computers. It is built around the MYC-JX8MX CPU Module and has brought out rich peripherals through connectors and headers such as 4 x USB 3.0 Host ports and 1 x USB 3.0 Host/Device port, Gigabit Ethernet, TF card slot, USB based Mini PCIe interface for 4G LTE Module, WiFi/BT, Audio In/Out, HDMI, 2 x MIPI-CSI, MIPI-DSI, 2 x LVDS display interfaces, NVMe PCIe M.2 2280 SSD Interface, etc. It is provided with both Linux and Android software package and delivered with necessary cable accessories for customer to easily start development as soon as getting it out-of-box. A MIPI Camera Module MY-CAM003 is provided as an option for the board.

More information can be found from MYIR's website:

MYD-JX8MX Development Board | i.MX 8M ARM Board-Welcome to MYIR 

MYD-JX8MX Top-view

                     MYD-JX8MX Bottom-view

评论

Where will I get the source code of this ? 

I have same question as Abhilash. I did find on their website but can't find there official code repositories for this board :smileysad:

The board comes with a quick start guide which will provide user the download link for the software package and documentations.

无评分
版本历史
最后更新:
‎11-15-2019 01:23 AM
更新人: