rt1010 io的外部中断及外接flash操作

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rt1010 io的外部中断及外接flash操作

804 Views
1150666288
Contributor II

 1.rt1010  io口用作外部中断,去记录电机的霍尔反馈信号,该怎么做。

    

 2.通过flexspi外接了w25q32fv。按照例程,在flexspi时钟初始化时,会退出调试模式。原因是什么

Tags (1)
1 Reply

735 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 志成 项,

非常感谢使用NXP产品,很高兴为你提供技术支持!
1) I/O中断请参考SDK软件库中的input_interrupt例程
2) 对于这个问题,我不太清楚理解是否跟你一致,很多IDE都是支持代码运行在QSPI中调试的,所以我不太理解你说的的‘退出调试模式’是如何发生的,请解释一下。

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------