reset adc input voltage range from 3.3v to 5v

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

reset adc input voltage range from 3.3v to 5v

647 Views
z_zhou
Contributor I

Hi nxp,

I use the MIMXRT106x-evk board to read some data in the adc channel. I check the datasheet, the max input voltage can be decided by Vref. The default setting is 3.3v represented of 4096 step. How could I change its max range from 3.3v to 5.0V?

Kind regards

Labels (1)
Tags (2)
0 Kudos
1 Reply

551 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Zhou Zhou,

Please refer to Table 54 of the datasheet.

pastedImage_1.png

The maximum voltage allowed by Ref Voltage High is 3.6V, although is not recommended to work with the maximum voltage allowed, this is why by default comes with 3.3V. 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos