imxrt10xx bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt10xx bootloader

1,525 Views
ffloree
Contributor III

Hi,

do you have the source code of imxrt1052 bootloader? i want to copy application image from QSPI flash to SRAM.

i downloaded the mfgtool2 (Flashloader_i.MXRT1050_1.0_GA), i there isn't plugin bootloader source code.

Tags (1)
0 Kudos
Reply
2 Replies

1,095 Views
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 Kudos
Reply

1,095 Views
joanxie
NXP TechSupport
NXP TechSupport

for QSPI supporting, pls create salesforce case, then send the firwmare to you, I could'n upload this in public community.

summit salesforcehttps://community.nxp.com/docs/DOC-329745

0 Kudos
Reply