imx Rt595 I3C interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx Rt595 I3C interface

Jump to solution
623 Views
gilmotta2
Contributor II

Hello All,

Can anyone please share or point an I3C sample code for the RT595 to me? I would like to run a test sending bytes over I3C. I'm using the MIMXRT595-EVK and I did not find any sample code for this EVK.

Thanks,

Gil

#RT595

0 Kudos
1 Solution
612 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @gilmotta2 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, I'd like to refer to the I3C demo in the SDK for RT 595.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

View solution in original post

0 Kudos
2 Replies
593 Views
Mahesh_Chandra
NXP Employee
NXP Employee

Hi,

SDK has two projects. One project is set up for I3C master and the other project is set up for I3C slave.

You can directly use these projects after connecting two MIMXRT595-EVK boards together as mentioned

in the code examples.

0 Kudos
613 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @gilmotta2 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, I'd like to refer to the I3C demo in the SDK for RT 595.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

0 Kudos