iMXRT1176 XMCD Simplified Configuration to Full Configuration Migration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMXRT1176 XMCD Simplified Configuration to Full Configuration Migration

174 次查看
kurikuriken
Contributor I

Hi,

We are using the iMXRT1176 for our project. We use the SEMC SDRAM interface (similar to the Evk) and configure it using the xmcd. Currently we use the simplified configuration. We would like to migrate to using the full configuration since we want to adjust the SDRAM timing for spread spectrum as suggested in AN12879. In order to do this, we would like to know the default values for the various full configuration bits. What are the default values when we use the simplified configuration?

Thank you,

 

Ken

0 项奖励
1 回复

111 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @kurikuriken ,

 

Actually no default values for the simplified/full configuration, it depends on the board design indeed. We provide an example for SEMC SDRAM Simplified Configuration in the RM, you may refer to the following for details.

Kan_Li_0-1712808015611.png

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励