Dear Team,
My customer has a strange issue that his PC stops debugging RT1170-EVK and got the following issue :
---> here is the full log
Connection reset
at java.base/java.net.SocketInputStream.read(Unknown Source)
at java.base/java.net.SocketInputStream.read(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.readBytes(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.implRead(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.read(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.read0(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.read(Unknown Source)
at java.base/java.io.InputStreamReader.read(Unknown Source)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.receive(RedlinkServerClient.java:965)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1068)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1053)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1040)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.probeList(RedlinkServerClient.java:950)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.common.RedlinkServerEmuHandler.discoverEmulators(RedlinkServerEmuHandler.java:222)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.win.AbstractWinServerProbe.discoverEmulators(AbstractWinServerProbe.java:72)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.EmulatorsDB.getEmus(EmulatorsDB.java:260)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.EmulatorsDB.getEmulatorInfo(EmulatorsDB.java:200)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.EmulatorsDB.getAvailableEmulators(EmulatorsDB.java:129)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.TargetDiscovery.getAvailableEmulators(TargetDiscovery.java:499)
at com.nxp.mcuxpresso.core.debug.support.linkserver.launch.LinkServerLaunchConfigHandler.probeDiscovery(LinkServerLaunchConfigHandler.java:625)
at com.nxp.mcuxpresso.core.debug.launch.ProbeDiscoveryJob.run(ProbeDiscoveryJob.java:60)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
The customer has reinstalled all the drivers but still, this issue remains.
By the way, the board works fine on other PC.
Two questions:
1. Can you please advise what caused this issue and how to overcome it?
2. if the customer would like to use an external debugger such MCU-Link with RT1170-EVK. what is the correct process to do that?
Waiting for your kind feedback, Thanks in advance.
Regards,
Shai
Hi @shai_b ,
Normally, when you meet this issues, you just need to enter the serail download mode, and do the external flash mass erase.
You can follow this post:
The customer already make it works.
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
Dear @kerryzhou,
It looks like there is still an issue on this PC, the customer got the following error while using the NXP MCU Boot utility (see below)
as I said before if I will connect the EVK to another PC the EVK works (and debug works), but this issue appears only on this PC (of SW engineer).
Can you please advise what could be the issue here and how to resolve it?
Thanks in advance
KR,
Shai
Hi @shai_b ,
Seems you didn't read the following post in details:
Your board is MIMXRT1170-EVK, why you select RT500?
And do you use the correct USB port?