iMXRT1064 SNVS (RTC) Supercapacitor usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1064 SNVS (RTC) Supercapacitor usage

1,406 Views
johannzimmerman
Contributor III

Hello,

I am working on a project with iMXRT1064 on custom board.


The SNVS (RTC) input is supplied with a Gold Capacitor 0.22F.

Unfortunately it only lasts about 8 minutes.


IMXRT1064IEC on page 24 the maximum is specified with 0.25mA.


What is the typical average energy consumption of the SNVS (RTC) input if it is only supplied with 3.3V at VDD_SNVS_IN?
Can consumption be reduced?

Thank you

Johann

Labels (1)
0 Kudos
Reply
1 Reply

1,363 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Johann,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
When VDD_HIGH_IN > VDD_SNVS_IN, VDD_HIGH_IN will supply all the SNVS domain current and the current flows into VDD_SNVS_IN to charge the coin cell battery.
Please give a try.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply