I want to drive a 1280x800 pixel LCD at 60Hz on the iMXRT1052.
Is it possible?
If possible, please provide example parameters.
Hi Toru,
I recommend to check the following community post.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank your advice.
I'll ask a question to other community post.