iMXRT1050 can't find CM7_CFGxTCMSZ fields

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1050 can't find CM7_CFGxTCMSZ fields

ソリューションへジャンプ
422件の閲覧回数
shizj
Contributor III

I follow the AN12077 to demonstrate the FlexRAM configuration, but I can't find INT_xTCM_EN/CM7_CFGxTCMSZ fields in IOMUXC_GPR_GPR16/IOMUXC_GPR_GPR14 as section 2.1.2. shows.

Is there anything wrong?

shizj_0-1691405298693.png

AN12077 section 2.1.2

shizj_0-1691404855956.png

shizj_0-1691404943431.png

RM version: IMXRT1050RM Rev. 5, 09/2021

 

 

 

 

 

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
389件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

These fields appear as reserved because it was determined that the user should not modify them.
For testing FlexRAM reallocation I suggest you follow these steps: Reallocating the FlexRAM - NXP Community

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
1 返信
390件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

These fields appear as reserved because it was determined that the user should not modify them.
For testing FlexRAM reallocation I suggest you follow these steps: Reallocating the FlexRAM - NXP Community

Best regards,
Omar

0 件の賞賛