I am using the evkmimxrt1020 eval board and lwip_iperf_bm example from the SDK_2.5.0_EVK-MIMXRT1020. Only changing the ip address in the example source code, I get the following Bandwidth measurement over Ethernet.
Client connecting to 10.2.1.102, TCP port 5001
TCP window size: 85.0 KByte (default)
------------------------------------------------------------
[ 3] local 10.2.1.119 port 56990 connected with 10.2.1.102 port 5001
[ ID] Interval Transfer Bandwidth
[ 3] 0.0-10.1 sec 30.9 MBytes 25.7 Mbits/sec
I am running iperf v2.0.5 from my laptop connected over Ethernet as well.
Is this the maximum throughput I can expect from the mxrt1020?
Hi,
I checked with local i.MXRT product team and get below Ethernet throughput data with RT1050 product with iperf demo:
I got suggestion customer can use a strong performance PC to do the test.
Wish it helps.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------