i.mx rt 1062 SEMC DMA performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx rt 1062 SEMC DMA performance

3,034 Views
ivanosipov
Contributor II

Dear sirs.

I try now interfacing imxrt1060<-->FPGA via SEMC SRAM interface with sync mode 16 bit multiplexed Addr/Data.

I use DMA transfer to/from FPGA and have a quite large time gaps between bursts in transfer.

My used parameters:

AXI and SEMC frequencies 150MHz

SEMC sync mode, latency=3, burst=4(->burst 16 words)

DMA transfer size 1 KB, DMA granularity 32 bytes;

All of this functionally works, I can write, read and check results. Time diagrams inside the each burst seems OK.

But overall transfer speed is more then 2-x  less than expected.

We have this results (controlled by oscilloscope with CS pin):

150Mhz    WR    1KB    overall time=10us    burst16 time=140ns    gap time=170ns    speed=102.4MBps
150MHz    RD    1KB    overall time=10.5us    burst16 time=170ns    gap time=170ns    speed=97.5MBps

The best 1KB transfer time (in theory) must b:

32 {bursts} *(1{CS}+1{ADW}+3{latency}+16{burst}+1{/CS}+1{interval})*Tclk=4.9 us;

What causes our time gaps and how to eliminate/decrease it?

I attach a register dumps, captured just before DMA transfer launch, and ready to supply any other information if needed.

Thank you. Ivan.

PS:

I look at that threads for imx 6s, and can`t find any solution there...

.../thread/438098, .../thread/356944, .../thread/440832

Labels (1)
10 Replies

2,098 Views
nickwallis
Senior Contributor I

@Hui_Ma I too am interested in this topic, do you have any update on access to the linked document above? thanks.

0 Kudos

2,533 Views
ivanosipov
Contributor II

No answers several days, it`s sad...

I suspect, this problem can be a hardware restriction, I`d like to hear an answer from NXP support.

If I can do nothing to achieve expected peak throughput, I won`t waste my time on this.

Ivan.

0 Kudos

2,533 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ivan,

Sorry for the later reply.

We don't have SEMC performance data for external FPGA, while we have SEMC SDRAM as a reference.

Please check AN12437 about SDRAM performance data.  

pastedImage_1.png

SDRAM write performance better than read, for the write operation is pipelined.

For the DMA access could not enable DCache to increase Read performance, I think your test result is also reasonable.

Thanks for the attention.

best regards,

Mike

0 Kudos

2,533 Views
ivanosipov
Contributor II

Thanks a lot, Mike.

There is a interesting picture in AN12437, I mark red the points which I use in my case (as I can understand):

pastedImage_1.png

Maybe, you could explain some things (or know someone, who can).

Lets speak, as an example,  about DMA transfer from SEMC to OCRAM, the process can have a variants:

1. DMA reads 32bytes from SEMC via SIM_H7, and than writes 32bytes to OCRAM via SIM_H7

2. DMA organizes SEMC reading, OCRAM writing, and SIM_M7 converting between them.

i.e. reading and writing can be in parallel or sequential.

IF case #1 used, my time gaps are understandable. But doing such a loss of performance is so strange...

IF case #2, there are a chances to tune-up a process?

I can`t deal with only 50%, I want, at least, 80%.

Ivan.

P.S. I just now make a test with OCRAM<==>OCRAM DMA transfer (copy) 1 KB - time is 4us.

250 MBps copy = 500 MBps read + 500 MBps write (!!!).

It seems, no DMA engine, nor OCRAM connection are not a bottlenecks.

0 Kudos

2,533 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ivan,

SIM_M7 works as an arbitrator, which set access priority for masters (DMA, ENET, LCD and etc) to access Slave (OCRAM, SEMC connected external memory devices).

The working way is 1 as you listed:

 1. DMA reads 32bytes from SEMC via SIM_H7, and than writes 32bytes to OCRAM via SIM_H7

So, there needs DMA to do read and write accessing.

There with the bandwidth difference for OCRAM and SEMC SDRAM:

Max. speed for OCRAM : 64bit 133MHz

Max. speed for SEMC SDRAM: 16bit 166MHz.

Thanks for the attention.
Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

2,533 Views
ivanosipov
Contributor II

Hi Mike,

if we agree to previous, this does not explain, why gap time ( to act with relatively fast OCRAM) is equal or more then the (relatively slow)SRAM burst time. I do some measures about this. I vary CPU,IPG and SEMC frequencies and log the result time. Gap time depends on both IPG and SEMC clocks (violet).

pastedImage_1.png

My next questions maybe not to you personally, but to NXP support:

Can anybody please tell me, are this time gaps "normal" for this chip, or I can do anything to decrease them?

And, the second, is this performance drop the same in new RT 11xx series?

Thank you,

Ivan.

2,533 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ivan,

I would recommend to refer my colleague shared document about <iMXRTxxxx Memory Performance: ITCM / DTCM / OCRAM / SDRAM / FlexSPI (QSPI / HyperFLASH)> from here.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

2,533 Views
ivanosipov
Contributor II

Thank you Mike, but something goes wrong...

I can`t access this doc.  Ivan.

pastedImage_1.png

0 Kudos

2,533 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ivan,

I am checking with document author if that document could be shared.

I will update when I got any feedback.

best regards,

Mike

0 Kudos

2,533 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ivan,

That document is in preliminary status. 

The author still need more time to edit before released.

While, I couldn't make sure when it will be released.

Sorry for that. 

best regards,

Mike