i.MXRT1170 IO voltage before power up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1170 IO voltage before power up

Jump to solution
450 Views
Eugene3
Contributor II

Are there any IO pins to be allowed to input 3.3 voltage before applying CPU power?

 

0 Kudos
1 Solution
437 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 We don't recommend you power on any IO before the chip is powered on, the reason is:

When RT pin is powered on before than the POR, the leakage will cause the DCDC PSWITCH to high, it will open the POR, but, please note, it can't meet the datasheet POR sequence, especially the following item:
datasheet, chapter 4.2.1.1 Power-up sequence

kerryzhou_0-1696408734642.jpeg

 

Then, it will cause the VDD_SOC_IN no voltage, the core can't work, then the chip can't work.
So, you can't let the RT pin have voltage before the RT MCU POR.
To this situation, in fact, some other customer use this hardware to resolve it:
Have buffet IC between the RT chip and the other device control port, I2C, UART ,SPI and GPIO.
The other customer used buffet IC is tc74vcx125ft.

 

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
2 Replies
438 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 We don't recommend you power on any IO before the chip is powered on, the reason is:

When RT pin is powered on before than the POR, the leakage will cause the DCDC PSWITCH to high, it will open the POR, but, please note, it can't meet the datasheet POR sequence, especially the following item:
datasheet, chapter 4.2.1.1 Power-up sequence

kerryzhou_0-1696408734642.jpeg

 

Then, it will cause the VDD_SOC_IN no voltage, the core can't work, then the chip can't work.
So, you can't let the RT pin have voltage before the RT MCU POR.
To this situation, in fact, some other customer use this hardware to resolve it:
Have buffet IC between the RT chip and the other device control port, I2C, UART ,SPI and GPIO.
The other customer used buffet IC is tc74vcx125ft.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
420 Views
Eugene3
Contributor II

Hi @kerryzhou 

Thank you so much. Your information will help my design.

0 Kudos