请问自己找的4.3寸TFT LCD屏资源,与RK043FN02H-CT 的4.3寸 TFT屏接口基本一致的,如附件,就37腿不一样,但通过MIMRT1052-EVK Demo点不亮TFT屏,有哪些问题问题,如何排查?谢谢!
Hi George Li ,
楼主你好!
你看下你的LCD手册,你的XR, TP pin XR引脚是什么功能?
官方的板子37-40脚是悬空的,没有接其他的。
我不知道你LCD这些引脚的功能是什么, 触摸信号吗?
如果是触摸信号,按道理不会影响LCD显示。
如果真的不是LCD显示方面的引脚,你还是要看下你的时序参数,是否和官方的一致,这样好具体配置。
比如Hsync, Vsync, DCLK的频率等。
希望能帮到你,如果还有问题,欢迎继续交流!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------