i.MXRT1051DVL6A (A0 silicon): can 3V3 on DCDC_In damage part?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT1051DVL6A (A0 silicon): can 3V3 on DCDC_In damage part?

ソリューションへジャンプ
1,457件の閲覧回数
scott_thompson
Contributor III

I'm coming on-board to a new design using the i.MXRT1051DVL6A where the A0 silicon was specified in the BoM and the board was designed with 3V3 on the DCDC-In rail.

Looking in the datasheet, this rail appears to still have an Absolute Maximum rating that seems like it should withstand > 3V0 volts on DCDC-IN, but two boards that I'm working with draw so much current when 3V3 is put on the NVCC-* rails that the LDOs end-up current limiting and shunt the 3V3 rail to about 0.7V.

I've made a small mod where I put a diode in series to the DCDC-IN rail to try and limit it to ~3V but as soon as NVCC is connected the 3V3 rail tanks.

We can't wait for a board spin and are thinking of replacing the BGA MCU using a turnkey but wanted an opinion if 3V3 on A0 silicon will damage the MCU or if we should ensure that hardware mods are performed before powering-up the MCU after replacement.

I've isolated the SDRAM supply and the flash supply is connected to 3V3 directly; all told, it comes down to connecting the NVCC lines to the MCU where the overcurrent happens.

Any thoughts?

Thanks,

Scott Thompson, TC Helicon

1 解決策
1,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Scott

A0 erratum and datasheet (below) limited voltage to 3.0V, so 3V3 may damage chip

pastedImage_1.jpg

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,317件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Scott

A0 erratum and datasheet (below) limited voltage to 3.0V, so 3V3 may damage chip

pastedImage_1.jpg

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,315件の閲覧回数
scott_thompson
Contributor III

Thank you.  I was just coming in to check on the Errata for that mask.  Now I have something to hand-wave to.  Already have some A1 silicon on order to replace these guys.

Thanks for taking the time to answer my question.

Regards,

Scott Thompson, TC Helicon

0 件の賞賛