i.MXRT 1050 USB Host+Hub example project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT 1050 USB Host+Hub example project?

1,776件の閲覧回数
dav1
Contributor V

Is there a driver + example project available, demonstrating host-mode + multiple usb-devices running via a usb hub?

- Preferably where the hosted peripherals are 1050 evkits running the "USB Audio device class 2.0" example (HS mode)

0 件の賞賛
3 返答(返信)

1,343件の閲覧回数
b36401
NXP Employee
NXP Employee

i.MX RT 1050 includes 2 High Speed OTG controllers, which could be configured either as Host or as Device, being able to support HUB, depending of the included USB drivers of the used BSP.
Here is Linux BSP for i.MX RT1050 EVK:
https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,343件の閲覧回数
dav1
Contributor V

Hi Victor,

We're not using Linux (for realtime reasons), so my question is for a bare-metal / rtos implementation of USB-Host mode

---

Is there a driver + example project available, demonstrating host-mode + multiple usb-devices running via a usb hub?

- Preferably where the hosted peripherals are 1050 evkits running the "USB Audio device class 2.0" example (HS mode)

---

0 件の賞賛

799件の閲覧回数
sly1975
Contributor I

Hi,

Do you have a response about iMXRT 1050 USB Host+Hub example project ?

Thanks

 

0 件の賞賛