i.MXRT 1020 Connect to ROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT 1020 Connect to ROM

1,143 Views
vlad95vlad
Contributor I

Hello, I tried to connect to i.MXRT 1020 in custom board via LPUART using sdphost and command: sdphost.exe -p COM9 -- error-status. But i got following  error: unknown HAB mode 4036616662.
Status (HAB mode) = 4036616662 (0xf099e1d6) Unknown error code (4036616662). Error code changes every time. Also i used NXP-MCUBootUtility but it has the same problem. Could anybody explain to me the reason?

Regards.

Labels (1)
0 Kudos
Reply
4 Replies

1,120 Views
FelipeGarcia
NXP Employee
NXP Employee

Are you booting in Serial Downloader mode? I would make sure the BOOT_MODE pins are appropriately sampled.

Regards,

Felipe

0 Kudos
Reply

1,113 Views
vlad95vlad
Contributor I

It's Serial Downloader mode. There is no response for ping command now. I can read eFuses state and burn it. That's all. Also USB driver doesn't provide VID and PID. I had +3,3V on NVCC_PLL(72 pin  LQFP144) on a first powering up. Now the pin has a 0.1uF cap connected to GND. Could this accident have negative consequences for this MCU?   

vlad95vlad_0-1619178154457.png

 

1,098 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

NVCC_PLL is the 1.1V output of the same voltage that supplies digital portions of USB PHYs, PLLs, and the internal 24 MHz oscillator. Powering 3.3V through this pin is not acceptable and it could definitely damage your device.

FelipeGarcia_0-1619200642357.png

Best regards,

Felipe

0 Kudos
Reply

1,084 Views
Mikle_B
Contributor I

Hello, 

I'm also trying to  connect to my i.MXRT1020. This is my first experience with FreeScale-like MCU since I used LPC line before. I can read controller's ID via JTAG. When I'm trying to connect to serial port I have the same problem as Vlad do. USB connection does not works for me as well - Windows see device but can't recognize it, windows device manager shows VID is 0x0000 and PID is 0x0002 that isn't correct values. 

0 Kudos
Reply