i.MX1060 SDRAM issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX1060 SDRAM issue

4,095 Views
donghua_chen
Contributor I

Hello,

I want to change the setting of “DLL delay chain clock“.

In Rev 1 of the IMXRT1060RM, this can be done via DLLSEL and DQSSEL field of MCR register.

However, they are removed from Rev 2 of the reference manual. 

Please advise where we can set SDRAM read clock source to “DLL delay chain clock” and add more delay? thanks !

Labels (1)
0 Kudos
10 Replies

4,090 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) However, they are removed from Rev 2 of the reference manual.
Please advise where we can set the SDRAM read clock source to “DLL delay chain clock” and add more delay? thanks!
-- Actually, the SEMC module doesn't contain the DLLSEL and DQSSEL bits area, so they're removed in the updated version of RM.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

4,069 Views
donghua_chen
Contributor I

Hello,

Would like to check when DSQ mode (DSQMD=1) is configured to loopback from DSQ pad (B7) shown below,

  • Is capacitor C76 meant to control the read strobe delay?
  • What is the formula to calculate the delay? 
0 Kudos

4,087 Views
donghua_chen
Contributor I

Hi jeremyzhou,

Thank you for your quick reply.

if so, how to add more delay?

0 Kudos

4,066 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Please check the datasheet to figure the impact of DSQ mode on the SEMC timing specification.
1) How to add more delay?
-- What kind of delay or time do you want to add?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

4,012 Views
donghua_chen
Contributor I

Hi,

We are looking at delaying of DQS similar to FlexSPI input operation shown 1.jpg.

For SEMC/SDRAM input operation, the datasheet only specified the data input setup and hold time.  It does not mentioned how to configure the delay of DQS.   I cannot find any text on the capacitor connected to the DQS pad.

Please point me to the right paragraph that explain how the capacitor works when DQSMD = 0x01. 

We hope to add delay of 1 to 3 ns to SEMC_DQS by using the right value of capacitor.

thanks !

0 Kudos

4,007 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Actually, NXP recommends Flexspi_DQS and SEMC_DQS pads both be floating and do not used for other functions if external memory has not this DQS dedicated pin, and it's useless to connect the capacitor to the DQS pad of the above memory chip to add the delay time.
So I think you'd better refer to the datasheet of the external memory which has the DQS pin if you want to try to add the delay time, it may provide some guides to make it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos

3,997 Views
donghua_chen
Contributor I

Hi,

Our design and SDRAM selection were done based on the design of NXP RT1060 EVB.  Both SDRAM from ISSI and Winbond selected by NXP do not have DQS pin.

When DQS pin of i.MX RT1060 is recommended to be left floating, please confirm DQSMD should be set to 0x1 or 0x0?

We need to check the TIS spec accordingly.  When DQSMD = 0x0, TIS of 8.67ns (> Tclk166mHz 6.01ns) does not make sense.

0 Kudos

3,971 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
1) When DQS pin of i.MX RT1060 is recommended to be left floating, please confirm DQSMD should be set to 0x1 or 0x0?
-- You can set the DQSMD to 0x01 to achieve the maximum speed.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

3,958 Views
donghua_chen
Contributor I

Hi,

Setting DQSMD to 0x01 will not work with our design using the Winbond SDRAM at all.  Note that the same SDRAM was also used in i.MX RT106F vision solution.

About 8-10 months back, it was NXP FAE who told us to set DQSMD to 0x0 when we first tried to turn on this Winbond SDRAM.

Lastly, please comment that on TIS of 8.67ns when DQSMD is set  0x0.  How will 8.67ns work with Tac  (5 to 5.4ns) of any SDRAM in CAS 3 read operation?

The timings do not tally on paper but it worked with Winbond SDRAM when DQSMD is set to 0x0.

0 Kudos

3,953 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
TIS is used to demonstrate the input timing, so it's not fit for reading operation actually (as Fig 1 shows).

jeremyzhou_0-1613976490220.png

                                                                                           Fig 1

In further, after checking, the pins of W9825G6JB-6I is almost compatible with IS42S16160J-6BLI, and the SEMC can access the IS42S16160J-6BLI successful when DQSMD is set to 0x1, maybe you can give a try.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos