i.MX RT106F with 8080 panel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT106F with 8080 panel

440 Views
kentseng
Contributor II

Dear Sir

We develop a project using RT106F, but the LCM panel with 8080, 

have any RT106x with 8080 panel interface connection and example code?

Labels (1)
Tags (2)
0 Kudos
1 Reply

434 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Have any RT106x with 8080 panel interface connection and example code?
-- Whether you want to RT106x to connect the LCD panel via the 8080 interface, if yes, please refer to the application note for details.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos