i.MX.RT1052 - Is it possible to create a 32bit PWM module using 2 quad timers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX.RT1052 - Is it possible to create a 32bit PWM module using 2 quad timers?

Jump to solution
902 Views
Cindy
Contributor III

Hi,

Is it possible to generate a 32-bit PWM output using 2 quad timers?

in this post:-

https://community.nxp.com/t5/Digital-Signal-Controllers/32-bit-compare-with-the-Quad-Timer/m-p/82019...

xiangjun_rong mentioned that:-

"when you use Cascaded counter mode for T3, and T2 output is the tick for T3, the T3:T2 is NOT a standard 32bits single Timer"

My questions is:-

a) How to combine 2 quad timers to form a 32-bit PWM module if cascading 2 quad timers is not the way to do it?

 

Thank you.

 

Best Regards,

Cindy

Labels (1)
Tags (1)
0 Kudos
1 Solution
888 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1)Is it possible to generate a 32-bit PWM output using 2 quad timers?
-- No, the Quad Timer (TMR) doesn't support the feature.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
870 Views
Cindy
Contributor III

Thank you!

0 Kudos
889 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1)Is it possible to generate a 32-bit PWM output using 2 quad timers?
-- No, the Quad Timer (TMR) doesn't support the feature.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------