i.MX RT1050 with external 8/16-bit SDRAM and 8/16-bit SCL NAND flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX RT1050 with external 8/16-bit SDRAM and 8/16-bit SCL NAND flash

跳至解决方案
1,926 次查看
abertu
Contributor II

I want use the i.MX RT1050 with an external 8/16-bit SDRAM and an external 8/16-bit SCL NAND flash.
Are there some schematics to follow as reference?

Thanks in advance.
Angelo

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,570 次查看
abertu
Contributor II

For this issue, refers to IMXRT1050 reference manual, chapter 48.4.3.

Best regards,

Angelo

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,569 次查看
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 项奖励
回复
1,569 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Angelo,

In case of the SRAM implementation, you could refer to the i.MX RT1050 EVK. On the following link you could find the “i.MXRT1050 EVK Extended Feature Example Code and HW guide” where board schematics are included:

https://www.nxp.com/webapp/Download?colCode=i.MXRT1050-EX-CODE-AND-HW-GUIDE&appType=license

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,569 次查看
abertu
Contributor II

Dear Carlos,

thank you for your kindest answer.

I had already checked the archive "i.MXRT1050 EVK Extension Feature Example Code and HW Guide", but I find only info about CSI, FlexIO, FlexSPI, LPSPI, PWM, SPDIF and WiFi. Nothing about the SLC NAND Flash.

Best regards,

Angelo

0 项奖励
回复
1,571 次查看
abertu
Contributor II

For this issue, refers to IMXRT1050 reference manual, chapter 48.4.3.

Best regards,

Angelo

0 项奖励
回复