i.MX RT eLCDIF RGB Mode Use Case

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT eLCDIF RGB Mode Use Case

ソリューションへジャンプ
4,152件の閲覧回数
farid_mabrouk
Contributor II

I have run the evkmimxrt1060_elcdif_rgb example on my imx RT1060 dev board. Then I modified it based on this doc so that I can run the demo on a 1280x800 LCD: https://www.nxp.com/docs/en/application-note/AN12302.pdf 

after the modifications I did I get this message:

Debug1.png

This is how I configured my memory:

Debug2.png

ラベル(1)
0 件の賞賛
1 解決策
3,721件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

  Thanks for your updated information.

  If you can't meet the target of 60 frames per seconds, it is still related to the HSW, HBP, HFP, VSW, VBP, VFP data of your LCD, I find you are totally use the application note data, but you didn't refer to your own LCD datasheet data.

  In fact, I can't find the HSW, HBP, HFP, VSW, VBP, VFP data in the LCD file which you have shared.

  Still as my reply in the previous time:

pastedImage_1.png

   You need to find your own LCD controller related data, then define it in the code, and calculate the related video PLL output clock, and configure it in your project.

   Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
30 返答(返信)
3,123件の閲覧回数
farid_mabrouk
Contributor II

My LCD is 1280x800 and it does not need Vsync and Hsync. It only uses DE ( data enable.)

The issue I’m having now is that I can’t meet the target of 15 frames per second even if I’m using 16 bits color depth pixel.

How can I optimize my eLCDIF speed so that I can have 15 frames/second. The frame buffers are stored in 8MB non-cacheable SDRAM.

Thank you in advance for your help!

0 件の賞賛
3,123件の閲覧回数
farid_mabrouk
Contributor II

I figured out how to set the master bit, please see below:

void APP_ELCDIF_Init(void)
{
    const elcdif_rgb_mode_config_t config = {
        .panelWidth    = APP_IMG_WIDTH,
        .panelHeight   = APP_IMG_HEIGHT,
        .hsw           = APP_HSW,
        .hfp           = APP_HFP,
        .hbp           = APP_HBP,
        .vsw           = APP_VSW,
        .vfp           = APP_VFP,
        .vbp           = APP_VBP,
        .polarityFlags = APP_POL_FLAGS,
       //.bufferAddr    = (uint32_t)s_frameBuffer[0],
        .bufferAddr    = (uint32_t)BframeBuffer,
        .pixelFormat   = kELCDIF_PixelFormatXRGB8888,
        .dataBus       = APP_LCDIF_DATA_BUS,
    };

    ELCDIF_RgbModeInit(APP_ELCDIF, &config);

    APP_ELCDIF->CTRL|= 1<<5 ;
    APP_ELCDIF->CTRL2 = 0x00700000;

}

Any comments?

0 件の賞賛
3,123件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

 If you search the RT RM LCD register, you will find MASTER is the LCDIF_CTRLn[MASTER] bit.

 

Best Regards,

Kerry

0 件の賞賛
3,123件の閲覧回数
farid_mabrouk
Contributor II

Hi Kerry! I checked with the lcd manufacturer and found that vsync and Hsync signals need to be pulled low or set to logic low. How can I change these pins yo logic low. I’m assuming once the eLCDIF peripheral is initialized, these signals will be pulled up high. How do I make sure vsync and Hsync are pulled low at all times? 

Thanks 

0 件の賞賛
3,123件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

  Do you mean, the vsync and hsync signals, need to be always low in your LCD? if yes, you don't need to configure the related RT code to these pins, you can connect your HSYNC and VSYNC pins in the LCD directly to the GND.

Best Regards,

Kerry

0 件の賞賛
3,123件の閲覧回数
farid_mabrouk
Contributor II

1. I don't think I set master bit to 1; how do I do that, and which register is it?

2. Could you please let me know how you guys configure the pixel clock. I took the example of generating a frequency of 70.5 MHz as it is, but I need to now how did this turn out to be the case when you used these clock functions:

/* * 000 derive clock from PLL2 * 001 derive clock from PLL3 PFD3 * 010 derive clock from PLL5 * 011 derive clock from PLL2 PFD0 * 100 derive clock from PLL2 PFD1 * 101 derive clock from PLL3 PFD1 */ CLOCK_SetMux(kCLOCK_LcdifPreMux, 2); CLOCK_SetDiv(kCLOCK_LcdifPreDiv, 0); CLOCK_SetDiv(kCLOCK_LcdifDiv, 0);

3. is there any limitation of the selection of posdivider, and loop divider below?

/ * Initialize the Video PLL. * Video PLL output clock is OSC24M * (loopDivider + (denominator / numerator)) / postDivider = 70.5MHz. */ clock_video_pll_config_t config = { .loopDivider = 47, .postDivider = 16, .numerator = 0, .denominator = 0, };


 

0 件の賞賛
3,123件の閲覧回数
farid_mabrouk
Contributor II

I will make sure I will get the HSW, HBP, HFP, VSW, VBP, VFP from the LCD maker. In the meantime, can you tell me if I memcpy() function instead of the nested for loop would make any difference?

Also according to the App note: "Configure the eLCDIF AXI master feature register to improve the performance for 1280 × 800 LCD in the sd_jpeg.c. # In the bottom of function “void APP_ELCDIF_Init(void)”, add the line: APP_ELCDIF->CTRL2 = 0x00700000;"

I added the above line of code at the end of my void APP_ELCDIF_Init(void) function, and it just made my code stop running. Any comments on this suggestion?

Cheers!

0 件の賞賛
3,123件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

  If you already prepare the frame buffer, I think you can use the memcpy,You totally can try it on your side.

   About your APP_ELCDIF->CTRL2 = 0x00700000; stop running problem.

 Do you set MASTER bit to 1?

  You can check it on your side.pastedImage_2.png

   Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
3,123件の閲覧回数
farid_mabrouk
Contributor II

Hello Kerry!!

i managed to solve y issue by disabling CachI and CachD; however, I was not able to meet the target of 60 frames per seconds using the function: App_fill_framebuffer, which uses a nested for loop. Could you please suggest how this code can be optimized for speed. Remember I’m using 1280x800. 

Thanks 

0 件の賞賛
3,722件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

  Thanks for your updated information.

  If you can't meet the target of 60 frames per seconds, it is still related to the HSW, HBP, HFP, VSW, VBP, VFP data of your LCD, I find you are totally use the application note data, but you didn't refer to your own LCD datasheet data.

  In fact, I can't find the HSW, HBP, HFP, VSW, VBP, VFP data in the LCD file which you have shared.

  Still as my reply in the previous time:

pastedImage_1.png

   You need to find your own LCD controller related data, then define it in the code, and calculate the related video PLL output clock, and configure it in your project.

   Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
3,131件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

   You heap and stack size is not the same as the application note, please modify the size like the AN, stack size is 0X8000, heap size is 0x800000.

pastedImage_1.png

Others, I still need more time to check details, will reply in the next week, because now I already out of work.

Thanks a lot for your understanding.

Best Regards,

Kerry

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

Hi Kerry!

 I hope you can help me on this issue. Now my rgb code is running from the SDRAM. As I mentioned in my previous discussion, I modified evkmimxrt1060_elcdif_rgb so that it can run on  a 1280x800 LCD. I sent you the data sheet in my previous posts. Now my issue is that I am seeing these signals: HSYNC, VSYNC, LCD_EN, and LCD_CLK (which I configured to be 70.5MHz). But I am not seeing any data on the data lines( R[0..7], G[0..7],B[0..7]). These signals are all pulled low when I check them with a scope. However, in a different test when I configured these data lines as GPIOs, I was able to toggle them. I don' t know if there is any register I need to access to enable data lines, if so please tell  me. In the meantime, I attached below a copy of my code, please have a look and let me know if I am missing any configuration. I am just suspecting the SRDAM boot up to be the issue but I am not sure, as I am able to see the clocking signals. I also verified and I found that I am getting frame buffer fall at 60 Hz frequency.

Please help!

Attached project:

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

More investigation of the problem leads me to suspect that my main issue is the graphics data that I stored in the Cachable SDRAM memory space. I have 8MB of data per frame and that cannot be stored in the 2MB of non-cachable SDRAM memory space. As I declared  my frame buffer as a global variable, it just got initialized to zero and that's why I am seeing a black screen all the time.

If I need to prevent this frame buffer data from being cached what should I do? the example I was looking at was dealing with a 2MB of data which got stored as non-cachable and that was it.

I hope someone can comment as soon as possible.

Cheers!

0 件の賞賛
3,132件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

   You can disable the cache, then test it directly.

   Comment :

    SCB_EnableDCache();
    SCB_EnableICache();

  In BOARD_ConfigMPU();

  Then you don't need to care about your non-cachable memory is not enough, just test it to check whether your problem is related to the cache.

BTW, please share me your hardware schematic, I really need to know how you connect LCD to the RT chip.

  

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

Do you see any issue in my code in the way the SDRAM is configured. Also I don't know if I need to align my data: do 64 bytes align?

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

Any Updates?

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

Images deleted 

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

These are my schematics screenshots

0 件の賞賛
3,132件の閲覧回数
farid_mabrouk
Contributor II

Any issues with schematics?

0 件の賞賛
3,132件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andre marcus,

  Could you please give me your RT schematic picture which used to connect your LCD pins?

  I just need to check it, because I need to know which RGB signal you have connected, if your schematic is important, you don't need to send me the whole file, you just need to give me some picture about it, just like this:

pastedImage_2.png

Then I can help you more details.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛