flexSPI_B1外接QSPI Nor Flash启动问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexSPI_B1外接QSPI Nor Flash启动问题

1,927 Views
cams
Contributor I

Hi,在我的项目应用中采用i.mxRT1062,由于flexSPI_A用做了其它复用端口,只能用flexSPI_B1作为外部QSPI Nor Flash存储接口,QSPI Nor Flash 采用GigaDevice GD25Q54C,MDK 的 led_blinky 中如何设置在Nor Flash 中进行调试以及Flash Loader如何设置?,其与flexSPI_A1设置有何不同?谢谢!

Labels (1)
0 Kudos
3 Replies

1,621 Views
jeremyzhou
NXP Employee
NXP Employee

Hi rayandy fan ,

非常感谢使用NXP产品,很高兴为你提供技术支持!
1.硬件连接参考参考手册中的Table 8-1. ROM Bootloader Peripheral PinMux。
2. 修改工程XIP文件夹内的evkbimxrt1060_flexspi_nor_config.c以匹配GD25Q54C。
3. 根据考参考手册中的Table 8-10. Fuse definition for Serial NOR over FlexSPI,调整Fuse中的BOOT_CFG值或BOOT 引脚状态来匹配GD25Q54C。
3. 至于你说的设置Flash Loader,不太明白你的意思,请再解释一下。

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,621 Views
cams
Contributor I

非常感谢您的答复!我现在有个问题,根据rt1060参考手册ROM APIs特殊说明,bootROM是不是只允许从flexSPI1 A端口启动,其它flexSPI 端口不支持(比如flexSPI1 B、flexSPI2)? 所以我通过flexSPI1 B端口外接QSPI Nor Flash是否就不能通过bootROM启动?rt.jpg

0 Kudos

1,621 Views
jeremyzhou
NXP Employee
NXP Employee

Hi rayandy fan ,

感谢回复。
FlexSPI ROM API不代表ROOM boot启动有这方面的限制,但说实话,我也不能100%确定的,所以我的建议是你可以考虑Table 8-1. ROM Bootloader Peripheral PinMux给出的Secondary option连接方式,如果跟你其他的硬件电路部分不冲突的话。

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos