modified the imxrt 1060 evk board to test HyperRam. debug fails with following messages after that.
error log:
Thu Nov 12, 2020 23:59:00: IAR Embedded Workbench 8.50.6 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)
Thu Nov 12, 2020 23:59:00: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\NXP\iMXRT.dmac
Thu Nov 12, 2020 23:59:00: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\NXP\iMXRT_Trace.dmac
Thu Nov 12, 2020 23:59:01: None of the application was placed in flash memory.
Thu Nov 12, 2020 23:59:01: Downloaded C:\Users\manikkoth\Desktop\work\uClinux_IMXRT1060\keil_projects\sdk_imxrt1060\boards\evkmimxrt1060\driver_examples\flexspi\hyper_bus\polling_transfer\iar\
debug\flexspi_hyper_flash_polling_transfer.out to flash memory.
Thu Nov 12, 2020 23:59:01: 0 bytes downloaded into FLASH (0.00 Kbytes/sec)
Thu Nov 12, 2020 23:59:01: Loaded macro file: C:\Users\manikkoth\Desktop\work\uClinux_IMXRT1060\keil_projects\sdk_imxrt1060\boards\evkmimxrt1060\driver_examples\flexspi\hyper_bus\polling_transfer\
iar/evkmimxrt1060.mac
Thu Nov 12, 2020 23:59:01: Loading the CMSIS-DAP driver
Thu Nov 12, 2020 23:59:01: Probe: CMSIS-DAP probe SW module ver 1.21
Thu Nov 12, 2020 23:59:01: Probe: Connecting to CMSIS-DAP:0229000006d0b02700000000000000000000000097969905 firmware v.1.10
Thu Nov 12, 2020 23:59:01: Emulation layer version 4.67
Thu Nov 12, 2020 23:59:01: Notification to init-after-power-up hookup.
Thu Nov 12, 2020 23:59:01: CoreSight error: Cannot read IDCODE. No SWD access. Debugging is not possible.
Thu Nov 12, 2020 23:59:01: CMD_INTERPRETER: failed
Thu Nov 12, 2020 23:59:01: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\NXP\iMXRT.dmac(169,19): Error: Operation error.
Thu Nov 12, 2020 23:59:01: Error while calling macro execUserProbeConnect
Thu Nov 12, 2020 23:59:01: Notification to core-connect hookup.
Thu Nov 12, 2020 23:59:01: CPU status FAILED
Thu Nov 12, 2020 23:59:01: LowLevelReset(system, delay 200)
Thu Nov 12, 2020 23:59:04: Fatal error: Failed to connect to CPU Session aborted!
Thu Nov 12, 2020 23:59:05: Cannot initialize DAP access.
Thu Nov 12, 2020 23:59:05: IAR Embedded Workbench 8.50.6 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)
Thu Nov 12, 2020 23:59:05: Loading the CMSIS-DAP driver
tried running a known project as well. right now board has hyperRam mounted.
Hi vinaymanikkoth,
What's your selection in the below now?
OPTION1: USE Hyperflash( DNP R153~R158, Mount R356,R361~R366)
OPTION2: USE QSPI FLASH(Mount R153~R158, DNP R356,R361~R366)
MIMXRT1060-EVK is using the QSPI option2 in default, do you already modify it?
If you already modify option2 to option1, please modify back to option2, then try to connect with the QSPI flash, any progress or not?
BTW, do you have external JLINK or not?
If yes, you can use the external JLINK and the JLINK commander to connect your board, can you find the ARM core or not?
Best Regards,
Kerry
nothing changed.
is there any way to verify MCU is powering-up properly ?
can i get the sample device so that i can try to replace the MCU ?
Hi vinaymanikkoth
I have told you, you use the external JLINK to check your chip with the JLINK commander through the JTAG interface, whether the ARM core can be found or not.
Eg:
Please check it at first.
Best Regards,
Kerry
Hi vinaymanikkoth
Do you have the NXP LPC-LINK2? That tool also can used as the JLINK.
BTW, you need to use the SWD interface, not the JTAG, the RT chip in default using the SWD interface.
Best Regards,
Kerry
Hi vinaymanikkoth,
Do you refer to the AN12239 application note about How to Enable HyperRAM with i.MX RT?
https://www.nxp.com/docs/en/nxp/application-notes/AN12239.pdf
The software project is:
https://www.nxp.com/docs/en/nxp/application-notes-software/AN12239SW.zip
Do you use the same hyperRAM as this application note?
Do you use this project directly, and debug it? If you are using the RT1060, this project should works OK on your board directly.
Wish it helps you!
Any updated information, please kindly let me know.
Kerry