cmsis svd file for MIMXRT685S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cmsis svd file for MIMXRT685S

1,150 Views
mcuBoy
Contributor I

Dear Sir:

     I've searched everywhere and can't find the cmsis svd file for MIMXRT685S , can you tell me where to get it?

 

Thank You!

Best Wishs!

     

Labels (1)
0 Kudos
2 Replies

1,126 Views
Masmiseim
Senior Contributor I

Hello mcuBoy,

 

it is included in the SDK (devices\MIMXRT685S\ MIMXRT685S_cm33.xml) which you can download from here:

https://mcuxpresso.nxp.com/en/welcome

 

you can also get it from here:

https://github.com/Masmiseim36/nxpSDK/blob/master/devices/MIMXRT685S/MIMXRT685S_cm33.xml

 

Best Regards

0 Kudos

1,121 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The peripheral/register description file is named MIMXR685S_cm33.xml and it's located within the SDK in the following path: <SDK_EVK-MIMXRT685 path>\devices\MIMXRT685S\MIMXRT685S_cm33.xml
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------