Hi !
brief : we have a device (not NXP) that read JedecID from external flash thru SPI
here is the Valid transaction on logic analyzer:
you can see that the frequency of the transaction
now, we want to do the same with NXP MXRT1050.
we have managed to read the JedecID of the external device using help from forum:
Solved: Re: Read JedecID, erase & program external indepen... - NXP Community
but when we are sampling with the analyzer the SPI transactions to read JedecID we get this:
or this:
these looks like non valid transactions
we thought this is because the NXP works in high frequency so analyzer cant read it
how we can reduce the frequency? we need the SPI transaction will look like the first picture, from our old device.
when I try to set Flex SPI clock to 25 it shows an error:
the project is a modified flexSPI_nor_polling example project.
Thanks
Adi
Intel
已解决! 转到解答。
Hello
Hope you are well.
With the default configuration, it will be difficult to reach the 25Mhz so I suggest you change the clock that sources the FlexSPI clock. I used the SEMC clock source to reach this frequency.
Please refer to this configuration:
CLOCK_SetMux(kCLOCK_FlexspiMux, 0x0) this function with the value of 0x0 sets SEMC as source for FlexSPI clock.
If you have more questions do not hesitate to ask me.
Best regards,
Omar
Hello
Hope you are well.
With the default configuration, it will be difficult to reach the 25Mhz so I suggest you change the clock that sources the FlexSPI clock. I used the SEMC clock source to reach this frequency.
Please refer to this configuration:
CLOCK_SetMux(kCLOCK_FlexspiMux, 0x0) this function with the value of 0x0 sets SEMC as source for FlexSPI clock.
If you have more questions do not hesitate to ask me.
Best regards,
Omar