Writing to a qspi flash config register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing to a qspi flash config register

514 Views
jautry
Contributor IV

Was working on a new platform design using the iMXRT1062.  Was working as expected with 128MB but when I went to a 256MB and 512MB flash, things started breaking.  Assumed it was the 3 byte and 4 byte addressing issue but am having trouble reading the bank config register to set 4 byte mode.  I modified the flexspi_nor_polling_transfer example application to test out access but does not seem to work.  Perhaps someone can see what is in error

Additions to LUT

/* Write Bank register */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITE_BANKREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x17, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x01),

/* Write NV Bank register */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITE_NVBANKREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x18, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x01),

Bank register write procedure:

status_t flexspi_nor_bank_vwrite(FLEXSPI_Type *base, flexspi_port_t port, uint8_t vol, uint8_t writeData)
{
uint8_t seq = vol;
status_t status;
flexspi_transfer_t flashXfer;
flashXfer.deviceAddress = 0;
flashXfer.port = port;
flashXfer.cmdType = kFLEXSPI_Write;
flashXfer.SeqNumber = 1;
flashXfer.seqIndex = vol;
flashXfer.data = writeData;
flashXfer.dataSize = 1;

/* Write neable */
status = flexspi_nor_write_enable(base, 0);

if (status != kStatus_Success)
{
return status;
}

status = FLEXSPI_TransferBlocking(base, &flashXfer);

if (status != kStatus_Success)
{
return status;
}

status = flexspi_nor_wait_bus_busy(base, kFLEXSPI_PortA1);

return status;
}

Tags (3)
0 Kudos
1 Reply

489 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, whether you can tell me which QSPI flash you used.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos