Will an FlexSPI AHB read access to flash check the busy bit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will an FlexSPI AHB read access to flash check the busy bit?

1,423件の閲覧回数
mitterha
Senior Contributor I

Hello,

I was just wondering if an AHB read access to flash with FlexSPI will check if the flash is ready before it attempts to read data from flash.

For example if I send a chip erase command and do not wait until the erase is completed instead attempt to read 1kByte from the same flash by AHB, will the FlexSPI peripheral poll the flash busy bit and wait with the read command until the erase is finished?

Kind regards,

Stefan

0 件の賞賛
8 返答(返信)

1,251件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan Mitterhauser,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
There is no software configuration or polling need for the AHB command except FlexSPI initialization. AHB master access external flash device transparently similar as normal AHB slave.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,251件の閲覧回数
mitterha
Senior Contributor I

Hello Jeremy,

what happens if the flash is busy for 50 seconds because I'm erasing it and after the first second I try to read 1kByte of the device in AHB address range? Will FlexSPI wait 49 seconds before it reads the flash device, will it generate an error or will it return 1kByte of zeros because there is no response from external flash device?

Kind regards,

Stefan

0 件の賞賛

1,251件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan Mitterhauser,

Thanks for your reply.
1) Will FlexSPI wait 49 seconds before it reads the flash device?
-- Yes, It will wait until the previous command completes, because the CPU prefetch the code via 64bit AHB Bus (i.e. AHB command), code program calls FlexSPI driver to erase or program Data Flash via 32bit IPS Bus (i.e. IP IP command).
The ARB_CTL arbitrator will determine which kind of command will preemptive the control to be the ARB command when they both want to handle the flash. And only one command is serviced at that time.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,251件の閲覧回数
mitterha
Senior Contributor I

Hello Jeremy,

the ARB_CTL will only wait until the erase command is sent over the bus - which won't take long, but will it check the busy flag of the flash to see if the flash has finished erasing before it allows the next flash command to execute?

Kind regards,

Stefan

0 件の賞賛

1,251件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan Mitterhauser,

Sorry for reply late.
1) The ARB_CTL will only wait until the erase command is sent over the bus - which won't take long but will it check the busy flag of the flash to see if the flash has finished erasing before it allows the next flash command to execute?
-- Yes, I think so.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,251件の閲覧回数
mitterha
Senior Contributor I

Hello jeremyzhou‌,

did you get more information from the design team?

Kind regards,

Stefan

0 件の賞賛

1,251件の閲覧回数
mitterha
Senior Contributor I

Hello Jeremy,

could you please verify this with the design team so we won't run into any timing problems in our product?

Kind regards,

Stefan

0 件の賞賛

1,251件の閲覧回数
mitterha
Senior Contributor I

Hello jeremyzhou‌,

did you get any more information?

Kind regards,

Stefan

0 件の賞賛