When I don't need the TX_ER output, can it be used with GPIO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When I don't need the TX_ER output, can it be used with GPIO?

Jump to solution
619 Views
george
Senior Contributor II

Hi All,

My customer uses KSZ8081MNX with RT1170.

george_0-1693147243374.png

The KSZ8081MNX doesn't need the TX_ER signal, so my customer wants to use that pin as a GPIO.

I think that's perfectly fine, but my customer wants a comment from NXP.
Could someone please comment on that certainty?

Can the TX_ER pin be used as a GPIO?
It doesn't affect the behavior of ENET, right?

Thanks,
George

0 Kudos
1 Solution
505 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @george ,

  Your understanding is totally correct!

   To the RT chip, if the pin is not used by the peripherial, it can be configured as the GPIO function.

  So, you can use it as the GPIO when you don't use it as the ENET function.

 

Wish it helps you!

If you still have question about this case, just kindly let me know.

If your question is solved, please tell me to mark the correct answer, just to close this case.

Any new issues, welcome to create the new case.

Best Regards,

Kerry

View solution in original post

0 Kudos
3 Replies
506 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @george ,

  Your understanding is totally correct!

   To the RT chip, if the pin is not used by the peripherial, it can be configured as the GPIO function.

  So, you can use it as the GPIO when you don't use it as the ENET function.

 

Wish it helps you!

If you still have question about this case, just kindly let me know.

If your question is solved, please tell me to mark the correct answer, just to close this case.

Any new issues, welcome to create the new case.

Best Regards,

Kerry

0 Kudos
488 Views
george
Senior Contributor II

Hello @kerryzhou,

Thanks for your comment.

BR,
George

0 Kudos
485 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @george ,

  You are always welcome!

   If your question is solved, please help to mark the correct answer, just to close this case.

  Any new issues, welcome to create the new case, thanks.

Best Regards,

kerry

0 Kudos