Wdog timeout reset problem after usb resume from suspend

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wdog timeout reset problem after usb resume from suspend

726 Views
eric_yp_chen
Contributor I

Hey @jeremyzhou 

I've design a product which both need watch dog and usb selective suspend function.

Wdog timeout always triggered after resume  state.

I did add these setting during wdog init.

wdog_config.enablePowerDown = true;
wdog_config.workMode.enableStop = true;
wdog_config.workMode.enableWait = true;

 

Have you ever met this before ?

Any other register should I set before enter suspend ?

Or how to disable WDOG properly before enter suspend ?

Eric

0 Kudos
3 Replies

708 Views
eric_yp_chen
Contributor I

Hi @jeremyzhou 

Yes, you're right. I want to disable it.

0 Kudos

704 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and clarification.
After confirming, once the WDOG is activated, it must be serviced by the software on a periodic basis, it won't be able to be disabled prior to trigger reset event.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

712 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, I'm a bit confused with your question, it seems that you want to forbid or disable Wdog trigger a reset event after the USB has resumed from suspend function, isn't my understand right? I hope you can explain it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos