Hi,
Why is the WDOG1 still counting back to zero while I am debugging?
Also in the WDOG SDK example, I experience the same problem.
/*
* wdogConfig->enableWdog = true;
* wdogConfig->workMode.enableWait = true;
* wdogConfig->workMode.enableStop = false;
* wdogConfig->workMode.enableDebug = false;
* wdogConfig->enableInterrupt = false;
* wdogConfig->enablePowerdown = false;
* wdogConfig->resetExtension = flase;
* wdogConfig->timeoutValue = 0xFFU;
* wdogConfig->interruptTimeValue = 0x04u;
*/
WDOG_GetDefaultConfig(&config);
config.timeoutValue = 0xFU; /* Timeout value is (0xF+1)/2 = 8 sec. */
config.enableInterrupt = true;
config.interruptTimeValue = 0x4U; /* Interrupt occurred (0x4)/2 = 2 sec before WDOG timeout. */
WDOG_Init(DEMO_WDOG_BASE, &config);
PRINTF("--- I add a breakpoint here, wait for >10 seconds and WDOG triggers ---\r\n");
Read the last statement in the snippet above. I added a breakpoint there. After 10+ sec the watchdog triggers.
Shouldn't this take care of that?
* wdogConfig->workMode.enableDebug = false;
snippet from fsl_wdog impl
void WDOG_GetDefaultConfig(wdog_config_t *config)
{
assert(NULL != config);
/* Initializes the configure structure to zero. */
(void)memset(config, 0, sizeof(*config));
config->enableWdog = true;
config->workMode.enableWait = false;
config->workMode.enableStop = false;
config->workMode.enableDebug = false;
config->enableInterrupt = false;
config->softwareResetExtension = false;
config->enablePowerDown = false;
config->timeoutValue = 0xffu;
config->interruptTimeValue = 0x04u;
config->enableTimeOutAssert = false;
}
解決済! 解決策の投稿を見る。
Hi @kerryzhou
Nah, that's not true.
A Guide to Watchdog Timers for Embedded Systems | Interrupt (memfault.com)
Nevermind, found it myself
when I set the bool to true it works
config.workMode.enableDebug = true;
Thanks !
Hi @bp1979 ,
As you know, the watchdog is the hardware IP module, so, when you enable the WDOG, then the hardware timer will counting, if you don't feed it(refresh the counter), it will be overflow.
It is the correct result.
Best Regards,
Kerry
Hi @kerryzhou
Nah, that's not true.
A Guide to Watchdog Timers for Embedded Systems | Interrupt (memfault.com)
Nevermind, found it myself
when I set the bool to true it works
config.workMode.enableDebug = true;
Thanks !