Hi All
I checked VDD_USB_3V on the evaluation kit,
On one kit it is 2.5V on the other 2.6V,
Is this ok? Why it's not 3.0V?
Best
Hello,
I measured the I.mxrt1050 EVKB for it. And find the voltage is 2.62v. Depends on the RM(The output of the regulator can be programmed in 25 mV steps, from 2.625V to 3.4 V .) . So it it ok. Hope it help you. Have a nice day.
Best regards
never-displayed