Use RT116x in place of RT117x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use RT116x in place of RT117x

跳至解决方案
740 次查看
mrd
Contributor III

Could someone please confirm that a board designed for RT1176/RT1175 could instead use an RT1166/RT1165 as long as firmware only uses the resources only available on the RT116x part?

If so, let me know if this is spelled out in a document or video somewhere that I've overlooked on NXP's website.

0 项奖励
1 解答
735 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Thank you for your interest in the NXP MIMXRT Product, I would like to provide service for you.
RT116X is pin to pin compatible to the RT117X.
So, to the RT1176/RT1175 board can use the RT1166/RT1165, but your related application should use the RT116X code.
As you know, RT117x has more function than the RT116X, even the core frequence also higher than RT116X.
About the document, you an refer to your used chip reference manual the datasheet.
About the code, you can use the SDK:
https://mcuxpresso.nxp.com/en/select

Wish it helps you!
If you still have questions, please kindly let me know.
Best Regards,
kerry

在原帖中查看解决方案

0 项奖励
1 回复
736 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Thank you for your interest in the NXP MIMXRT Product, I would like to provide service for you.
RT116X is pin to pin compatible to the RT117X.
So, to the RT1176/RT1175 board can use the RT1166/RT1165, but your related application should use the RT116X code.
As you know, RT117x has more function than the RT116X, even the core frequence also higher than RT116X.
About the document, you an refer to your used chip reference manual the datasheet.
About the code, you can use the SDK:
https://mcuxpresso.nxp.com/en/select

Wish it helps you!
If you still have questions, please kindly let me know.
Best Regards,
kerry

0 项奖励