Hi
With the SDK config tool I get theese warnings:
Issue: Unsupported version of the PWM Driver in the toolchain/IDE project. Required: 2.1.0, actual: 2.2.1.
Issue: Unsupported version of the SAI Driver in the toolchain/IDE project. Required: 2.2.1, actual: 2.3.1.
I am suprised that the versions of each module is not compatible with echother in the SDK.
The procect seems to compile, so it must be minor changes to the updatede drivers.
Is it safe to ignore?
Kasper
解決済! 解決策の投稿を見る。
Hi Kasper,
So you are importing a configuration from a different project to the new created project? If so, then that is the cause of the warnings. These peripherals were initiated using old version of the drivers so there is a mismatch with the new SDK drivers.
To get rid of this warnings please remove the SAI and PWM component and create them again in the same project using config tools.
Best regards,
Felipe
Hi Kasper,
Could you please provide the SDK and SDK version you are working on? Also please provide the version of the MCUXpresso IDE you are using.
I recommend you to update to latest version so you do not have this kind of problems but if you are using latest then please provide how can I replicate this on my side with the information requested above.
Best regards,
Felipe
Hi,
I am using the MIMXRT1064DVL6A.
Kasper
Hi Kasper,
I have imported same version of drivers in a project of MIMXRT1064-EKV using MCUXpresso IDE v11.2.1 and I cannot see this warning. Could you please provide how can I replicate this issue on my side?
Regards,
Felipe
Hi
Sorry for the delay.
I have attached a mex file from my project, and a document describing how I can create a new project with the same problem, inclusive the warnings/errors. Finally a folder with the resulting project (SDK-files must be refreshed(generated).
I have upgraded the SDK to the new version 2.8.5 with same result.
Hope that there is a reason for my problems.
BR
Kasper
Hi Kasper,
So you are importing a configuration from a different project to the new created project? If so, then that is the cause of the warnings. These peripherals were initiated using old version of the drivers so there is a mismatch with the new SDK drivers.
To get rid of this warnings please remove the SAI and PWM component and create them again in the same project using config tools.
Best regards,
Felipe
I had to remove the components from the config tool. I have tried to remove the SDK component with no success.
Also solved the problem with the USB.
The rest is just annoying warnings. I only need the "Record" channel for the SAI interface, so the config tool should not complain that the "Play" TX pins was not routed.
Thanks