I'm working with a FreeRTOS and USB. When I build the application to run out of internal ram (the default memory map) it runs as expected; however, as soon as I try to put portions of the map into SPI-based ram it gets wonky. I realize that certain memory blocks of USB need to be in DTCM, and after a lot of digging I found that I needed to set two macros in CFLAGS...
-DDATA_SECTION_IS_CACHEABLE=1 -DUSB_STACK_USE_DEDICATED_RAM=1
with that; however, the compile fails because middleware/usb/device/usb_device_ehci.c checks for USB_STACK_USE_DEDICATED_RAM and fails. I commented out the error and started down the road of trying to get this to work with a slightly more complicated memory map, but have not had any luck.
What is the reason for erroring out if USB_STACK_USE_DEDICATED_RAM is set?
Note: I am running with SDK2.14.0, running with evkmimxrt1060. Example code: SDK_2.14.0_EVK-MIMXRT1060/boards/evkmimxrt1060/usb_examples/usb_device_cdc_vcom/freertos)
已解决! 转到解答。