Things to check when connecting MIMX1160-EVB and MIPI OLED panel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Things to check when connecting MIMX1160-EVB and MIPI OLED panel

618件の閲覧回数
sukyeong
Contributor III

hi, i am using the board MIMX1160-EVK.

Originally, I used the LCD(RK055AHD091) provided by nxp, but I want to connect an OLED Panel to that part.

I want to display the OLED screen, but the screen doesn't come out.

Can you tell me what I need to check?

 

Here's what I did first:

I'd appreciate it if you could let me know what's wrong or what needs to be added

  • Hardware connection

(MIPI DSI DN0,MIPI DSI DP0,MIPI DSI DN1,MIPI DSI DP1,MIPI DSI CLKN, MIPI DSI CLKP

, LCD_RST_B, LCM_PWR_EN)

  • Write initialization code according to the changed driver

 

 Thank you.

0 件の賞賛
3 返答(返信)

601件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

Is the OLED panel has the same frame size and timing requirement as RK055AHD091? If it's different, you should modify the code in display_support.c.

 

Regards,

Jing

0 件の賞賛

595件の閲覧回数
sukyeong
Contributor III

Let's review it. By the way, if the board only supports 2 lanes, is it not compatible with 4 lanes of AMOLED?

タグ(1)
0 件の賞賛

577件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

Yes, if the OLED can't configure to 2 lane, RT1176 can't support it.

 

Regards,

Jing

0 件の賞賛