Secure JTAG in imxrt1060-evk using JLink base

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure JTAG in imxrt1060-evk using JLink base

2,212件の閲覧回数
Min1
Contributor I

Hello.

I'm using imxrt1060-evk. The board has MIMXRT1062DVL6A processor.

I want to use secure jtag so I followed AN12419 manual.

I did the fuse configuration described in the manual.

fuse configuration.PNG

 

here is my board & debugger connection. 

I'm using J-Link Base. I connected it to J21.

Power is supplied by DC 5V connection( J2). To use J2, J1 is connected to 1-2.

board_debugger connection.jpg

Here is my JLinkScript.

int InitTarget(void) {
  int r;
  int v;
  int Key0;
  int Key1;

  JLINK_SYS_Report("***********************************************");
  JLINK_SYS_Report("J-Link script: InitTarget() *");
  JLINK_SYS_Report(" NXP iMXRT, Enable Secure JTAG *");
  JLINK_SYS_Report("***********************************************");

 JLINK_SYS_MessageBox("Set pin JTAG_MOD => 1 and press any key to continue...");

  // Secure response stored @ 0x600, 0x610 in eFUSE region (OTP memory)
  Key0 = 0xa2631407; //I modified it to my eFuse value
  Key1 = 0x00e33510; //I modified it to my eFuse value

    JLINK_CORESIGHT_Configure("IRPre=0;DRPre=0;IRPost=0;DRPost=0;IRLenDevice=4"); //I modified IRLenDevice to 4
  CPU = CORTEX_M7;

  JLINK_SYS_Sleep(100);

  JLINK_JTAG_WriteIR(0xC); // Output Challenge instruction

// Readback Challenge, Shift 64 dummy bits on TDI, TODO: receive Challenge bits on TDO
  JLINK_JTAG_StartDR();
  JLINK_SYS_Report("Reading Challenge ID....");

  JLINK_JTAG_WriteDRCont(0xffffffff, 32); // 32-bit dummy write on TDI / read 32 bits on TDO
  v = JLINK_JTAG_GetU32(0);
  JLINK_SYS_Report1("Challenge UUID0:", v);

  JLINK_JTAG_WriteDREnd(0xffffffff, 32);
  v = JLINK_JTAG_GetU32(0);
  JLINK_SYS_Report1("Challenge UUID1:", v);

  JLINK_JTAG_WriteIR(0xD); // Output Response instruction

  JLINK_JTAG_StartDR();
  JLINK_JTAG_WriteDRCont(Key0, 32);
  v = JLINK_JTAG_GetU32(0);
  JLINK_SYS_Report1("Response key:", v);
  JLINK_JTAG_WriteDREnd(Key1, 24);
  v = JLINK_JTAG_GetU32(0);
  JLINK_SYS_Report1("Response key:", v);


  JLINK_SYS_MessageBox("Change pin JTAG_MOD => 0, press any key to continue...");

  return 0;
}

 

Here is my J-Link result. 

I thought Secure JTAG will be unlocked by using jLinkScript above.

However, unlocking failed and J-Link reported the wrong UUID.

J-Link also reported that it failed to power up DAP.

How can I solve it??

jlink result.PNG

 

0 件の賞賛
9 返答(返信)

2,200件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Min1 

Some points you have missed:

1. JTAG mode modification.

kerryzhou_0-1626834825537.png

You need to remove R323, R309, R152 as it connect the JTAG pins to the ENET PHY chip.

In fact, before your test the secure JTAG, you need to make the JTAG works at first, but now you already write the SJTAG.

 

2. From the AN12419, you missed this steps:

Finally, the user must program 0x1 in the eFuse SJC_RESP _LOCK to disable read/write access of the secret
response key. After this operation, the secret response field “SJC_RESP” becomes “invisible” in the fuse map. See
Figure 3 and Figure 4 .

kerryzhou_1-1626834944421.png

I don't know whey you modify your script :

JLINK_CORESIGHT_Configure("IRPre=0;DRPre=0;IRPost=0;DRPost=0;IRLenDevice=4"); //I modified IRLenDevice to 4

You can use the default:

JLINK_CORESIGHT_Configure("IRPre=0;DRPre=0;IRPost=0;DRPost=0;IRLenDevice=5");

You just need to modify the key0,key1 to your own fuse data.

Not long ago, I help one customer test the RT1050 SJTAG, it works OK:

https://community.nxp.com/t5/i-MX-RT/Secure-JTAG-in-imxrt1050-EVKB/m-p/1293040/page/2

Normally, I test the SJTAG, will let the JTAG work at first, then add the SJTAG.

You can add the above two missed points and test it again.

BTW, SW7 should be:1-off,2-off, 3-off, 4-on serial download mode.

1-OFF, 2-OFF,3-ON, 4-OFF, internal boot mode

Any updated information, just kindly let me know.

Kerry

 

 

 

0 件の賞賛

2,188件の閲覧回数
Min1
Contributor I

Hello. @kerryzhou 

Thank you for your answer.

I followed your step but failed again.

1. I edited eFuse configuration like the pic below.

fuse configuration edit.PNG

 2. removed R323, R309, R152

remove resis.PNG

 3. modified JLink Script

asdfasf.PNG

 

 

 

 

 

 

 

 

 

 

 

 

but the JLink result is failed.

jlinkkk.PNG

The Challenge UUID & response key is still wrong.

0 件の賞賛

2,185件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Min1 

 Do you use your JLINK base to connect the MIMXRT1060-EVK board before you modify the fuse?

I mean, whether you can use your JLINK base to debug the RT1060 or not?

 In my memory, JLINK base may have limit to connect the RT1060, I am using the JLINK plus, so if you didn't use it to debug the RT chip previously, you can check with Segger side, just make sure your JLINK base can support the RT at first.

Any updated information, kindly let me know.

Best Regards,

Kerry

0 件の賞賛

2,157件の閲覧回数
Min1
Contributor I

Sorry for the late reply @kerryzhou.

I have JLink Plus too, so I tested secure jtag using link plus.

It failed again. However, I discovered another problem.

When I connect JLink to secure JTAG board, JLink discovered only 1 device in JTAG chain!

JLink didn't find other device. It found only ARM CoreSight JTAG which has 4 IRLen.

Is it right for JLink to find only one device when Secure JTAG is activated?

 

Best Regards,

Min

0 件の賞賛

2,151件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Min1 

  If just connect one device to the JTAG , I think find one device is correct.

 Now, your UUID still not correct? What about the JTAG_MOD pin, do you connect it to higher or low?

Best Regards,

Kerry

0 件の賞賛

2,147件の閲覧回数
Min1
Contributor I

First, It starts with JTAG_MOD= 0.

I connect JTAG_MOD pin manually like the pic below and connected it to DC 3.3  or GND to change pin value.

secure jtag.jpg

0 件の賞賛

2,145件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Min1 

   Before you run the jlinkscript, set the JTAG_MOD=1, then run the jlinkscript, the jlinkscript will tell you set it to 0, then you change MOD to 0.

   Please test it again.

   before you add the secure, do you test the JTAG at first, whether that works or not?

 

Best Regards,

KERRY

0 件の賞賛

2,143件の閲覧回数
Min1
Contributor I

Yes, JTAG worked before secure JTAG.

I set JTAG_MOD to 1 and followed script message but failed.

JLink reported error that Too few devices on the JTAG bus. IRPos: 0, TotalIRLen: 4 like the message.

Min1_0-1628487403822.png

etc. I didn't edit TotalIRLen in script.

Best Regards,

Min1

 

0 件の賞賛

2,138件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Min1 

https://community.nxp.com/t5/i-MX-RT/Secure-JTAG-in-imxrt1050-EVKB/td-p/1290923/page/2

This post add more details about my secure JTAG testing, it also has the wave.

  You also can check the JTAG wave, whether it is correct.

About the JLINKscript, I just modify the key data.

 

int InitTarget(void) {
int r;
int v;
int Key0;
int Key1;

JLINK_SYS_Report("***********************************************");
JLINK_SYS_Report("J-Link script: InitTarget() *");
JLINK_SYS_Report(" NXP iMXRT, Enable Secure JTAG *");
JLINK_SYS_Report("***********************************************");

JLINK_SYS_MessageBox("Set pin JTAG_MOD => 1 and press any key to continue...");

// Secure response stored @ 0x600, 0x610 in eFUSE region (OTP memory)
// Key0 = 0x87654321;
// Key1 = 0xedcba9;
Key0 = 0x00000000;
Key1 = 0x87654321;

JLINK_CORESIGHT_Configure("IRPre=0;DRPre=0;IRPost=0;DRPost=0;IRLenDevice=5");
CPU = CORTEX_M7;

JLINK_SYS_Sleep(100);

JLINK_JTAG_WriteIR(0xC); // Output Challenge instruction

// Readback Challenge, Shift 64 dummy bits on TDI, TODO: receive Challenge bits on TDO
JLINK_JTAG_StartDR();
JLINK_SYS_Report("Reading Challenge ID....");

JLINK_JTAG_WriteDRCont(0xffffffff, 32); // 32-bit dummy write on TDI / read 32 bits on TDO
v = JLINK_JTAG_GetU32(0);
JLINK_SYS_Report1("Challenge UUID0:", v);

JLINK_JTAG_WriteDREnd(0xffffffff, 32);
v = JLINK_JTAG_GetU32(0);
JLINK_SYS_Report1("Challenge UUID1:", v);

JLINK_JTAG_WriteIR(0xD); // Output Response instruction

JLINK_JTAG_StartDR();
JLINK_JTAG_WriteDRCont(Key0, 32);
JLINK_JTAG_WriteDREnd(Key1, 24);

JLINK_SYS_MessageBox("Change pin JTAG_MOD => 0, press any key to continue...");

return 0;
}

 

0 件の賞賛