Is there an example/ guide available for an SDRAM bootable image on the RT1052?
I have tried to convert one of the SDK sample project into SDRAM bootable image but unable to boot from flash
SDK example projects (which has ethernet-wifi, LWIP, AWS, and Iot module)
I have noticed, if project is based on the “ethernet / wifi” or LWIP” the SDRAM boot issue arise (irrespective of Flash memory ).
Thanks
Hello James,
Hope you are doing well.
I recommend to begin with the following document:
https://community.nxp.com/docs/DOC-340655
It provides the steps necessary to create the bootable image for sdram.
Best Regards,
Sabina
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------