Hello community,
In Table 58-2. of the IMXRT1170 Reference Manual, SAI4 MCLK source is shown only SAI4_MCLK (pin).
Is SAI4_MCLK(pin) mean that clock source for SAI4 can use only external clock from SAI4_MCLK pin?
The other hand, SAI4_MCLK_DIR bit of GPR2 General Purpose Register, it can select input/output direction for SAI4_MCLK (12.4.4.4.3 Fields).
And Table 15-2. System Clocks Table inform about sai4_mclk_in2 and sai4_mclk_in3 but no more information about sai4_mclk_in2 and sai4_mclk_in3.
Is it possible to set a source other than external clock for SAI4_MCLK?
I look forward to hearing from you.
Best regards,
Ishii.
已解决! 转到解答。
Hi @takayuki_ishii ,
Yes, it is confusing here. Because in SDK demo, BOARD_BootClockRUN() calls CLOCK_SetRootClock(kCLOCK_Root_Sai4, &rootCfg). And in clock config tools, it shows there are two SAI_MCLK.
I tested on my RT1170 EVK. When select the SAI4_MCLK_DIR to 1 and GPIO_LPSR_05 as SAI4_MCLK output, I can see 24M signal on the pin. That means SAI4 has two MCLK source, SAI_MCLK1 and SAI_MCLK2. SAI4->TCR2[MSEL] can select which one will be used. And the SAI_MCLK1 is from SAI4_CLK_ROOT, SAI_MCLK2 is from external clock pin (GPIO_LPSR_05 or GPIO_LPSR_00).
Detail of the SAI4_CLK_ROOT can be got from clock config tool.
The table 58-2 is not correct. I'll report this issue.
Regards,
Jing
Hi @takayuki_ishii ,
Yes, it is confusing here. Because in SDK demo, BOARD_BootClockRUN() calls CLOCK_SetRootClock(kCLOCK_Root_Sai4, &rootCfg). And in clock config tools, it shows there are two SAI_MCLK.
I tested on my RT1170 EVK. When select the SAI4_MCLK_DIR to 1 and GPIO_LPSR_05 as SAI4_MCLK output, I can see 24M signal on the pin. That means SAI4 has two MCLK source, SAI_MCLK1 and SAI_MCLK2. SAI4->TCR2[MSEL] can select which one will be used. And the SAI_MCLK1 is from SAI4_CLK_ROOT, SAI_MCLK2 is from external clock pin (GPIO_LPSR_05 or GPIO_LPSR_00).
Detail of the SAI4_CLK_ROOT can be got from clock config tool.
The table 58-2 is not correct. I'll report this issue.
Regards,
Jing
Hello @jingpan
Thank you for your evaluation work..
I understand that SAI4_MCLK1 can use intanal clock as SAI4 clock source.
And The table 58-2 is not correct.
I will update this information to customer.
Best regards,
Ishii.