In my quest to know what is required to rebuild the Azure RTOS library using the IAR tools, I read the following post:
https://community.nxp.com/t5/LPC-Microcontrollers/Azure-ThreadX/m-p/1444008
Microsoft provides the IAR project files needed to build the library. Why doesn't NXP include them? NXP is behind the latest Github release so I downloaded the same release from Github to compare against. The only difference I can see is that tx_initialize_low_level.s is being supplied as tx_initialize_low_level.c. Otherwise every other file is the same.
It should be relatively easy to modify Microsoft's project files to reflect the tx_initialize_low_level.c change and include them in the NXP release. Is there a reason why this isn't being done?
Regards,
Greg
解決済! 解決策の投稿を見る。
Hi @gcary
The Azure RTOS library could be compiled in IAR. Here is a path for the IAR project file.
boards/evkmimxrt1160/azure_rtos_examples/
├── filex_lib
├── netxduo_lib
├── threadx_lib
└── usbx_lib
Please let me know if you need further information.
Regards
Daniel
I don't see a reason why there would be a problem if I compiled my own libraries, but I don't like to assume that is the case. Maybe NXP had some issues with doing that, so they decided to exclude those files? There could be a good reason the project files are not provided. Is there any reason I should not compile them myself?
Hi Daniel,
Thank you very much for helping out with this. I don't know if this will be helpful or not, but I wanted to let you know how ST Micro implements it in their STM32CubeMX software. I'm not saying they're doing it right. I'm only offering it as a comparison.
I created a sample project that only included ThreadX. The IAR project that it created did not use libraries. Every RTOS source file was included in the project. I compiled it, and after it was compiled I modified the top level user source file. I compiled the project, and the only file that needed recompiling was the one I modified. I was looking to see how much time the IAR tools took to inspect the status of all the RTOS source files. It did not take hardly any time at all.
I realize there are pros and cons to using libraries vs. source code files. But one thing I proved to myself is that recompiling speed doesn't appear to be an issue.
Regards,
Greg
Hi @gcary
The Azure RTOS library could be compiled in IAR. Here is a path for the IAR project file.
boards/evkmimxrt1160/azure_rtos_examples/
├── filex_lib
├── netxduo_lib
├── threadx_lib
└── usbx_lib
Please let me know if you need further information.
Regards
Daniel
Thank you Daniel! I never specified which processor I am using. I am using the RT1062, and unfortunately that EVK does not have the library build files.
I downloaded a variety of different SDKs just now, and the library projects are included in the RT116x and RT117x SDKs. The RT10xx projects that I downloaded do not have them.
Are their plans to update the SDK builds for the RT10xx to include the library build files for IAR?
Regards,
Greg
Hi Daniel,
I'm sorry, I see they are there. I just didn't know where to look before. Now I know. Thank you for showing me.
Regards,
Greg