RT1176 transfer data through usart at baudrate 921600

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 transfer data through usart at baudrate 921600

Jump to solution
1,015 Views
wangfan_1987
Contributor I

Hi:
I have a large mount of data to transfer through usart,so I need a high speed baudrate.But I meet some problem when change the baudrate.

  1. In the baudrate 115200 and 460800,the usart work well,I got the "hello world".
  2. When I try to change the baudrate in BOARD_InitDebugConsole() defined by the macro BOARD_DEBUG_UART_BAUDRATE to 921600,I got a garbled code.

I want to know how much is the top baudrate of the usart?Can I do some changes to make the usart work normally.

0 Kudos
1 Solution
665 Views
Padi-2023
Contributor III

1702628466529.png
After reading NXP data for an afternoon, please refer to LPC55S1x/LPC551x User manual "UM11295.pdf", I tried to use 1000000bps, RT1176 development board can work normally.

View solution in original post

11 Replies
666 Views
Padi-2023
Contributor III

1702628466529.png
After reading NXP data for an afternoon, please refer to LPC55S1x/LPC551x User manual "UM11295.pdf", I tried to use 1000000bps, RT1176 development board can work normally.

556 Views
wangfan_1987
Contributor I
Since the core frequency of IMXRT1176 is relatively high, configuring it with a baud rate of 921600 should not be a problem. If there are no issues at a baud rate of 1M, then the hardware communication on the circuit board should also be fine. This is a peculiar phenomenon. Nevertheless, thank you for your solution.
0 Kudos
955 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @wangfan_1987 

I did the testing myself and it works correclty, I only changed the macro value just like you did.

Can you help me sharing the value of the BAUD register?

You can access it while debugging, on the peripherals.

Miguel04_0-1695849452573.png

 

Best Regards, Miguel.

0 Kudos
940 Views
wangfan_1987
Contributor I

Thanks for your reply!

My Test board is MIMXRT1176-EVK REVA1,used a USB cable connect the board to PC to transfer usart1 data.

My test program is D:\wangfan\NXP\MIMIX1176\SDK_2_12_0_MIMXRT1170-EVK\boards\evkmimxrt1170\rtos_examples\freertos_hello\cm7

when run the program I want to get "48 65 6C 6C 6F 20 77 6F 72 6C 64 2E" ,which mean "hello world",while I get  "62 AC 3B B8 3E AC 3B 09 FF ".But in baudrate 115200,it was right.

The register value as following:

wangfan_1987_0-1695863652274.png

 

0 Kudos
927 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @wangfan_1987 

Can you share with me your IDE version? Your SDK version is 2.12, correct?

I'll look into it and let you know what I found.

Best Regards, Miguel.

0 Kudos
915 Views
wangfan_1987
Contributor I

Thanks for your reply! 

My IDE version is KEIL 5.33.0,My compiler is V6.15::ARMCLANG.The SDK pack  name is SDK_2_12_0_MIMXRT1170-EVK.zip,So I think it is the version.I am very thankful for your help!

0 Kudos
690 Views
Padi-2023
Contributor III

hi! I also encountered the same problem, so long you should have solved it! May I ask how it is solved? thanks.

0 Kudos
687 Views
wangfan_1987
Contributor I
Not sloved,just use a lower baudrate.Maybe core clock problem,if I have enough time,I will tyr to slove.:(
0 Kudos
685 Views
Padi-2023
Contributor III
I searched the NXP official website forum and found no solution, I think it is not supported to this piece, 24000000/921600=26.04166666667, 24000000\26=923076.923076, (923076.923076-921600) /921600*100%=0.16%, in fact, the error rate is 0.16%, according to this error rate can be used, even if the interface clock of kCLOCK_Root_Lpuart1 is raised, it may not be solved.
0 Kudos
681 Views
Padi-2023
Contributor III
Why do I think this is not supported by this piece? Since the RT685 I am using here is also set with this baud rate, no problems have been found so far
0 Kudos
859 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @wangfan_1987 

Thank you for the information, however you are using an outdated SDK version and another ide.

I'm using MCUXpresso IDE and this is recommended by NXP to use our platforms, I did not face any issue while using this IDE.

Best Regards, Miguel.

0 Kudos