RT1170 running both 100M and 1G ports at the same time on Zephyr

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1170 running both 100M and 1G ports at the same time on Zephyr

206 次查看
xuqincs
Contributor I

Hi,

Is it possible to use both 100M and 1G interfaces on RT1170 EVK at the same time on Zephyr?

I'm aware the 1G interface can use a 100M enet driver and get 100M speed, which is fine, but not able to get dhcp after enabling the enet1g node on DT, int-gpio, reset-gpio, etc are configured. Also, getting DT error if I enable enet and enet1g nodes at the same time. Zephyr seems already supports multi-enet interfaces, is there anything missing in the board DTS? We are using RT1170 EVK.

 

Thanks.

标记 (2)
0 项奖励
0 回复数