Dear support,
I am learning to program the RT11770-EVK device via the on-board debug probe with JLink firmware using command line tool JLinkExe v6.98e
I can connect from JLinkExe commander to the target correctly after issuing the "connect" command and select SWD connection type:
Connecting to target via SWD InitTarget() start InitTarget() end Found SW-DP with ID 0x6BA02477 DPv0 detected AP map detection skipped. Manually configured AP map found. AP[0]: AHB-AP (IDR: Not set) AP[1]: AHB-AP (IDR: Not set) AP[2]: APB-AP (IDR: Not set) AP[0]: Core found AP[0]: AHB-AP ROM base: 0xE00FD000 CPUID register: 0x411FC272. Implementer code: 0x41 (ARM) Found Cortex-M7 r1p2, Little endian. FPUnit: 8 code (BP) slots and 0 literal slots CoreSight components: ROMTbl[0] @ E00FD000 ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table ROMTbl[1] @ E00FE000 ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table ROMTbl[2] @ E00FF000 ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7 ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7 ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7 ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI ROMTbl[0][1]: E0043000, CID: B105900D, PID: 001BB908 CSTF Cache: Separate I- and D-cache. I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way SetupTarget() start FlexRAM configuration is restored syspll2 has been initialized already syspll2 pfd1 has been initialized already SDRAM init done SetupTarget() end Cortex-M7 identified.
However, I failed to download the target via loadfile command:
J-Link>r Reset delay: 0 ms Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit. ResetTarget() start DISPLAYMIX SRC reset CM7 SRC reset ResetTarget() end AfterResetTarget() start FlexRAM configuration is restored syspll2 has been initialized already syspll2 pfd1 has been initialized already SDRAM init done AfterResetTarget() end
J-Link>loadfile maestro_playback.bin No address passed for .bin file. Assuming address: 0x0 Downloading file [maestro_playback.bin]... Writing target memory failed.
I guess that the starting address parameter shouldn't be 0, but I can't find the right parameters to use as am I totally new to the RT1170-EVK device.
Please help to share some relevant materials so that I can follow.
Regards,
Yanfeng
解決済! 解決策の投稿を見る。
Hi,
It seems a bit weird, maybe the issue's related to the board itself, so you'd better check the board at first.
More further, did you ever try to debug the demo as the post shows? if not, please give it a try, especially for the LED blink demo.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to use a .srec file instead of .bin file or use the J-Flash to program the image file.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you for sharing JFlash tool, however it seems that I can't make it work with on-board debug probe running firmware: J-Link LPCXpresso V2 as the JFlash tool requires a license which I don't have.
Then I tried to program my app using the JLinkExe commander tool,
J-Link>loadfile iled_blinky_cm7.bin 0x30000000
Downloading file [iled_blinky_cm7.bin]...
...
J-Link: Flash download: Program & Verify speed: 397 KB/s
O.K.
However, after programming, I powered off the device and then power on it, there is no LED blinking.
Can you please let me know what should I do?
Regards,
Yanfeng
Hi,
Thanks for your reply.
1) Can you please let me know what should I do?
-- Firstly, you'd better check the bin is good, next, confirm the bin is programmed to chip, as the below figure shows.
By the way, I can program the bin file to the board and it also can boot up well.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Here I can see similar thing as your screen shot from JFlash tool, please see blinky-jflash.png attachment.
I did more tests here:
Firstly I tried a "debug" build .elf using gdb/JLinkGDBServer, and I run the program with break points and I can see the GPIO pin write function called correctly from gdb debugger. However, I never see the LED blinking correctly.
Then I tried a "flexspi_nor_debug" build using gdb/JLinkGDBServer, I noticed errors in GDB server side when gdb did "load" operation. However, after resetting these errors are gone. Eventually I got similar experience as the "debug" build.
I never saw blinky LED even though the app is downloaded to the device with Jlink tools via on-board probe.
Regards,
Yanfeng
Hi,
It seems a bit weird, maybe the issue's related to the board itself, so you'd better check the board at first.
More further, did you ever try to debug the demo as the post shows? if not, please give it a try, especially for the LED blink demo.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for the warm followups, it turned out that the board hardware was tweaked thus the default LED light doesn't blink. I tried on another board and it works now.
Sorry for all the trouble.
Regards,
Yanfeng