RT1060 Silicon revision question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1060 Silicon revision question

453件の閲覧回数
alessioschisano
Contributor III

Hi, I need to choose a MCU for an application, I see that MIMXRT106FDVL6B could be ok for my project, but checking on SDK to understand if the rev A1 is supported I see that only RT106x with rev A0 are supported. Is this a problem or I could use the SDK for MIMXRT106FDVL6A (rev A0) with the MIMXRT106FDVL6B (rev A1) ? Only final letter change

Thanks in advance

Ale

0 件の賞賛
1 返信

438件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is this a problem or I could use the SDK for MIMXRT106FDVL6A (rev A0) with the MIMXRT106FDVL6B (rev A1) ?
-- The SDK library is fit for either Rev A or Rev B actually.
Hope this is clear.
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛