RT1060 LUART1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1060 LUART1?

947件の閲覧回数
bw1
Contributor IV

The IMXRT1060RM document has the following note at the end of Table 8-2, page 196: 

NOTE
1. ...
2. The boot ROM enables LUART1 and USB1 interrupts in
serial downloader mode, and it disables these interrupts
before jumping to user applications. However, if the boot
ROM execution is interrupted by the debug tool, it cannot
disable these interrupts; the user application needs to
disable these interrupts in the startup codes.

Please clarify "LUART1" is this really just LPUART1?  LUART1 does not appear anywhere else in the document.  This note does not appear in the RT1050 reference manual either. 

ラベル(2)
タグ(2)
0 件の賞賛
1 返信

767件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Brad

yes "LUART1" is LPUART1. LPUART1 is also mentioned in Boot Chapter of

i.MXRT1050 Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛