RT1052 SAI and EDMA --- Dual Buffer Audio DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1052 SAI and EDMA --- Dual Buffer Audio DMA

1,176件の閲覧回数
zhang2015tz
Contributor I

I need a demo of dual buffer audio DMA. I noticed AN12090, which talks exactly what I need. But unfortunately, it seems like that AN12090 is an incomplete document. Dual buffer audio dma (ping pong buffer) needs a lot of DMA configurations. This document deosn't mention it at all.

So, does anybody know if there is the demo code for AN12090, and where to get it?

ラベル(1)
0 件の賞賛
1 返信

849件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ztz

one can find sai dma examples in  SDK_EVKB-MIMXRT1050 :

..driver_examples/sai/edma_transfer/sai_edma_tranfer.c
..devices/MIMXRT1052/drivers/fsl_sai_edma.c

Welcome | MCUXpresso SDK Builder 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛